STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to differentiate between STM32H743 and H745 at runtime?

Is there any way to find out if the code is executed on a H743 (single core) or a H745 (dual core) MCU at runtime?If I am not mistaken the DBGMCU_IDC (Identity code register) has the same value for both MCUs. Is there any other register which I could...

CHild.1 by Associate
  • 3186 Views
  • 6 replies
  • 0 kudos

When to trigger an outage

当我�?�时打开uart的接�?�中断和�?�一uart dma的接�?�中断时,两个中断都会被触�?�,如果设置的优先级相�?�,触�?�的顺�?是什么?

pLI.1 by Associate
  • 927 Views
  • 1 replies
  • 0 kudos

Resolved! How to trim the STM32 HSI easily

HelloI'm using a stm32L431 with an STLinkV3https://www.st.com/en/microcontrollers-microprocessors/stm32l4x1.html#documentationHSI is enabled at 16MHz for USART2, used to receive a 1200Bd signal.I receive wrong characters because of the trim.I underst...

po221 by Senior
  • 6352 Views
  • 11 replies
  • 0 kudos

STM32 SAI in TDM-4 Mode

Hi, Im trying to connect adau1772 using TDM-4 Protocol to an STM32 MCU (L462RE).Question 1: How to configure SAI as TDM-4, is my configuration wrong?Question 2: Correct callback which occures when data packed is received?Question 3: adau1772 is putti...

SYako by Associate III
  • 4079 Views
  • 5 replies
  • 0 kudos

capacitor does nut fully charge

hi I have a 1000uF capacitor and a blue pill STM32F103c8t6. I connected the positive end of cap to PB9 and the negative end to GND. then I had the code below inside while(1) loop///////////////////////////CHARGE////////////////////////////////// HAL_...

Ala by Senior
  • 2434 Views
  • 7 replies
  • 0 kudos

STM32L433 IWDG wakes up from SHUTDOWN Mode

In my use-case i want to have a watch-dog active when the device is in use to prevent software stucks or accidental ending in endless loops. Therefore i have configured the IWDG like this:void hw_IWDG_Init(void){   IwdgHandle.Instance = IWDG; IwdgH...

need help understanding Vref / Vdda

I'm trying to find what voltage reference my ADC is using, as it is not going up to 0xFFF. Along the line, I have become quite confused about the Vref - I used to use other chips where the Vref is just a reference voltage for the ADC, but with STM32 ...

deep_rune by Associate III
  • 17697 Views
  • 15 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.