STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L496RGT6 ADC

I'm having serious problems with the ADCI have the voltage I'm reading going through a 47K/100K voltage divider which feeds into an op-amp configured with a gain of 1 and then to ADC1Ch15 on PB0. VSSA is supplied from an external precision voltage re...

DCarr.1 by Senior
  • 2866 Views
  • 5 replies
  • 0 kudos

ADC on STM32L471RGT6 only returns 8 bit values

snippet from main code-> uint32_t a=0; uint32_t ADC_VAL[100]; ADC_VAL[0]=0; HAL_ADC_Start_DMA(&hadc1, (uint32_t*)&ADC_VAL, 1); HAL_Delay(10); a=ADC_VAL[0]; <- set a breakpoint at this point to view the value in 'a' <-      static void MX_ADC1_Init(v...

rwils.1 by Associate III
  • 2148 Views
  • 7 replies
  • 0 kudos

SPI communication with ADS1256 ADC data reading

In my project i have interfaced the STM32 nucleo-f446re dev kit with ADS1256 and when i trying to read the data there is no sclk ticking like transmitting 2 byte of data in logic analyzer there is no data transmission as well as no proper sclk tickin...

Pratyush by Associate II
  • 1803 Views
  • 0 replies
  • 0 kudos

configure system clock using registers for stm32f030k6t6

I need to configure the system clock using registers for 48mhz without external crystal, I already have it configured and tested with stmcube ide manager, but I need to decrease the flash memory and ram, as they are critical.i have this configuration...

0693W00000QNZsmQAH.jpg
jdo by Associate II
  • 4104 Views
  • 3 replies
  • 0 kudos

Problem with SWO in STM32H7B3I-DK board

I tried to redirect printf function to SWV. At first, I was not successful at doing so, until with some modifications and conditions it is working now:The core clock is 280 MHz but I have to set the core clock to 140 MHz in SWV configuration of CubeI...

0693W00000QNgk1QAD.png

Resolved! Hi, I need to implement a PID controller on my Nucleo board STM32G474RE, is there any developed library for this particular controller or resources available that help me to implement the PID controller?

The following document explains the DSP library for STM32F10x which contains the functions for the PID controller, is it compatible with STM32G474RE? If not, would you please guide me about its implementation on a microcontroller? https://community.s...

WKhan.2 by Associate II
  • 17579 Views
  • 4 replies
  • 1 kudos

CANFD not receiving data

HELLO EVERBODY i want to test the canfd communication on my nuclue-h753 in normal mode, my goal is to transmit data from canbus1 and receive it on canbus2 and vicaversa i configured both CANFD1 AND CANFD2 on the board with classic can configuration ...

abeba.1 by Associate III
  • 1206 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.