STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G0B1RET6 - Signal Trap error while debugging

I am getting this following error while trying to debug the Custom Board.please help me find out what is the meaning of this error.Thread #1 [main] 1 [core: 0] (Suspended : Signal : SIGTRAP:Trace/breakpoint trap) 0x1fff5a30 <signal handler called>(...

HPATH.1 by Associate II
  • 2280 Views
  • 2 replies
  • 0 kudos

Resolved! Vhys parameters for STM32F2xxx MCU I/O ports

What is the correct Vhys parameters for STM32F2xxx MCU I/O ports?It looks like as wrong datasheet values here (DS6329 Rev 18): https://www.st.com/resource/en/datasheet/stm32f207vg.pdf#page=102The published values are too big.Please double check the c...

0693W00000Suc2xQAB.png
Vuha by Associate II
  • 1210 Views
  • 1 replies
  • 0 kudos

How to properly start and reset timers?

I want to connect my MCU with a module which has a specific way of communication. Module sends messages of variable number of characters, where period between two characters is also variable. My idea is to use timer in order to overcome this problem....

NDjor.1 by Associate
  • 2089 Views
  • 1 replies
  • 1 kudos

STM32G474 Multi UART cant work with RingBuffer

I have fail using multi UART while using with the ring buffer,but using the HAL function testmulti uart is fine,i using the Keil c(MDK) complier check and i test if cnacel the HAL_UART_Init(&huart3) or other one is fine ,and i look for other of the s...

czack.1 by Associate
  • 812 Views
  • 0 replies
  • 0 kudos

STM32F091 RTC accuracy and measure error info.

Hi,​I would like to know about the STM32F091's RTC accuracy and frequency error information.Is the RTC accuracy or frequency error factor affected only by crystal?Is the RTC accuracy or frequency error factor affected by MCU itself?Is it any ST docum...

ElvisWei by Associate II
  • 1156 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H7 ADC using timers

Hello, I am using Nucleo-H743ZI ,I am using timer1 to trigger ADC.My APB1 clock frequency is 240MHz and my ARR register is 240 of timer 1. So my sampling rate of ADC should be 1Msamples/sec. To check it I am toggling a pin whenever ADC conver...

GHARI.1 by Associate II
  • 5805 Views
  • 13 replies
  • 0 kudos

using stm32f401rct6, two question, (1) system clock configured with a external 16Mhz crystal can work if it is set to 42Mhz but not at 84Mhz and (2) even if working will stuck at HAL_GetTick

(1) cannot run at 84Mhz, it will stuck at Error Handler RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_H...

JTse.1 by Associate II
  • 4092 Views
  • 10 replies
  • 0 kudos

STM32H745 - Dual core

I have few questions on STM32H745 dual core cortex M7 and cortex M4.i. What is the booting sequence when both the cores are enabled at the same time? Is there any application notes available in details.ii. How both the cores uses the same resource (R...

Monish by Associate
  • 2118 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.