Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi,I'm trying save some data into EEPROM after successful storage of first byte for second byte it goes to hard fault irq. Can anyone help me out from this issuevoid Save_data(float Data) { char Buff[15];unsigned long Address=0x08080000; sprintf(Bu...
I am using stm32cubeide
I tried to write the the register of LMX2595 through SPI using following API,here R1 is of 3 Bytes , 1 Address byte + 2 Data bytes;tData[3] = {0x07,0x30,0x0f}HAL_SPI_Transmit(&hspi1, tData, 4, 100);
Hey,I’m using a nucleo board: SMT32L031K6.I’m trying to make a simple bootloader but I’m struggling at unlocking the flash. In the reference manual it states that I must perform an unlocking sequence, but I haven’t been able to do it successfully. Wh...
Dear Sir.Using stm32u585 , The external clock on OSC32 pins is 32.768 Khz.I need to config LPTIM2 to run on 32.768 Khz with no success .How do I configure the SystemClock_Config() to make LPTIM2 to run on 32khz.Attached a code/** * @brief System C...
Hello Community,I'm currently working with STM32F429ZGT6 and going to fabricate pcbs for that. I also suspect that I may switch to STM32F746ZGT6 in future.So, I want to know will the same design be compatible for F746.Regards,Keshav Aggarwal
We are using STM32L071CBT6TR controller.We are receiving data through UART based on intterupt, for that we have enabled UART_IT_RXNE intterrupt.We have just enabled UART_IT_RXNE. But still we are getting frame error intterupt, we dont want frame erro...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.