STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STMP32H7 UART1 RS422 DMA Rx not functioning but Tx works.

Have STPM32H7 CPU running in 108 Mhz, and UART1 pull off PLL3 @50 Mhz, set baud rate at 3375000 with 8x oversampling rate.Do see the Tx signal by DMA (303 ns each baud ) out to device and replied with about 302 ns baud, signal is clean on the scope, ...

CWang.16 by Associate
  • 936 Views
  • 0 replies
  • 0 kudos

How does the STM32 Boot pin works?

I have a question about the BOOT pin performance of the STM32G031.In the datasheet says that upon reset, the boot pin (PA13) is established at the beginning as the picture shows. But I wanna know if it is only at the beginning of the reset and then I...

0693W00000VOdsnQAD.png
ECruz.2 by Associate
  • 9489 Views
  • 6 replies
  • 0 kudos

STM32F103 occasionally doubles counting speed in encoder mode

Hello!I use STM32F103 MCU Timer 2 in ecnoder mode. Ticks from an encoder go at approximately 1 MHz, so I use prescaler value 25 to decrease the frequency.Sometimes it works fine, but sometimes timer begins to count encoder ticks at double speed - it ...

MPopo.1 by Associate II
  • 4190 Views
  • 6 replies
  • 0 kudos

How do I resolve this issue - "arm-none-eabi-gcc: fatal error: cannot read spec file 'nano.specs': No such file or directory"?

Hi all,I hope someone can help me with this...If I remove the --specs=nano.specs in the MCU Settings tab, I get errors about #include_next files not found.If I install newlib I just errors about IO functions that I don't want...Kind regardsPG

PGump.1 by Senior III
  • 6872 Views
  • 2 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.