STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F401xB/C output a PWM signal on pin B14

So, the issue is as follows, according to datasheet the timer for pin B14 AF1, which is the PWM signal I believe, is the TIM1_CH2N. I have gone out of my way to try and output something, I just can't seem to understand what the problem is#define AF01...

MArdm.1 by Associate II
  • 1347 Views
  • 1 replies
  • 0 kudos

Resolved! I want to know how to use STM32F7XXX ADC_TRIPLEMODE_INTERL? I want to collect data from one io channel through three adcs to improve the sampling rate from 2.4M to 7.2M

HI,I'm new here.I found that three adc can be configured for alternate use by querying the STM32F7xxx datasheet.But But I have encountered some difficulties. I hope someone can explain it to me.Tell me how to use ADC_TRIPLEMODE_INTERL. The following ...

hhuan.21 by Associate II
  • 2371 Views
  • 2 replies
  • 1 kudos

scope question on variable wrt I2C ??

I have the following two wrapper functions:void POT_Load_Value(uint16_t value) { uint8_t w[2]; w[0] = 0; //reg w[1] = value; I2C_Write(POT_ADDR, w, 2); }   uint8_t I2C_Write(uint8_t device, uint8_t *pValues, uint8_t size) { if (HAL_OK == HAL_I2C...

SWenn.1 by Senior III
  • 976 Views
  • 1 replies
  • 0 kudos

In STM32G474 ,CORDIC module for trigonometric functions

In STM32G474 , I used CORDIC module for trigonometric functions calculations but this module requires fixed point represntation and i store the final value in float variable . can the transformations between fixed point to float point be done using a...

AIBRA.1 by Associate II
  • 1439 Views
  • 1 replies
  • 1 kudos

STM32F051K6 I want to set to 32bit TIMER for TIM2

Hi ,I am trying to set STM32F051K6  to 32bit TIMER for TIM2. what register needs to be set in-order to count to 32bit mode. I read the HRM but there is not detailed description where to set TIM 2 to 32bit mode.

ck.1 by Associate III
  • 1612 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.