STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32h745 SPI DMA not receiving the data

Hello,I am working on STM32h745 controller. I am using the DMA for SPI configuration. I declare the buffer in the RAM2 , transmission is done properly but I did not receiving the data on MISO why?/* MODIFICATION STARTS HERE */ .buffer(NOLOAD) : {  . ...

MDeva.1 by Associate II
  • 1428 Views
  • 1 replies
  • 0 kudos

Resolved! Openocd not able to flash a discovery board

UNEXPECTED ID code?, the discovery board is original.the onboard stlink is updated to latest version.If i google this Error, i get people trying to flash ST clone mcus, but mine is original. This is my openocd.cfg file:source [find interface/stlink.c...

0693W00000Y8fnkQAB.png
Javier1 by Principal
  • 2317 Views
  • 1 replies
  • 1 kudos

Resolved! Need help with flashloader/driver for STM32H7A3ZIT6Q with Octo-spi FLASH (twin quad) NOR flash MT25TL256

I have a custom board with an STM32H7A3ZIT6Q. It has the MT25TL256 NOR flash connected to the pins of OCTOSPI1.I'm trying to write a flashloader/driver.In our application we do not need to execute code from this flash. We only need it for data. But i...

Obejct Sensor Interfacing Doubt

Hello, I have tried to interface object sensor and all works well the object sensor led works perfectly when the range is close and far( LED is off when the path is blocked and vice versa). But I'm just getting stagnant ADC Values, it's stuck at 4095...

STM32F407 CAN filter doesn't work

Hi everyone.I have next problem. I trying to use CAN filter option, sometimes i need to configure them on fly. First basic filter its standard filter: /*CAN*/ canfil.FilterBank = 0; canfil.FilterMode = CAN_FILTERMODE_IDMASK; canfil.FilterFIFOAssignme...

OMarc.1 by Associate III
  • 2484 Views
  • 3 replies
  • 0 kudos

[SOLVED] Weak variables of global file scope linker error

So I'm trying to gain greater understanding on the STM32 tools on a project that I've inherited. I'm noticing that there are weak variables that are of global scope to a given file that are defined in multiple files such as follows:main.c:int g;other...

J.Christ by Associate III
  • 2032 Views
  • 4 replies
  • 0 kudos

Resolved! To read a word via I2C I need to add a second start condition to the procedure. What would be the easiest way to accomplish this?

From the datasheet from the slave device: "First the host must write a command to the slave device. Then it must follow that command with a repeated start condition to denote a read from that device's address. The slave then returns two bytes of data...

Resolved! Problem with configuring I2C1 (PB6 SCL, PB7 SDA) and specific GPIO outputs (PA5, PA6) on STM32L432KCUx, it may be bug, help needed.

Hi, i've been building self balancing robot, so i needed quite lot of periphelias to be working together, they are: I2C, EXTI's, two Timers in encoder mode, Timer in PWM generation mode and GPIO outputs.I'm using STM32CubeIDE 1.9.0., and STM32L432KC ...

0693W00000Y8W7VQAV.png

Store string into FLASH memory (STM32F407)

I want to insert the string my_data_SRAM in the base address of the FLASH. I wrote this code and tried 2 ways:1) *((uint8_t *)BASE_ADDRESS_FLASH+i) = my_data_RAM[i];2) HAL_FLASH_Program(TYPEPROGRAM_WORD, (uint32_t *)(BASE_ADDRESS_FLASH+i), my_data_RA...

luke514 by Senior
  • 3443 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.