STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Flash Memory: OCTOSPI feature with Quad SPI Flash

Hello,I am using the STM32H7B3LIH6Q with a MX25U51245GMI00 flash memory. The flash is only capable of using Quad SPI, not Octo SPI. If I wanted to use it, do I just use the Dual-Quad SPI mode in CubeMX to utilize it? Or would it not work at all?Also,...

0693W00000YA4hWQAT.png
KMew by Senior III
  • 5991 Views
  • 8 replies
  • 2 kudos

bh1750 sensor i2c poll method working fine but i2c DMA method not working with attached code . will DMA only transfer the value to global variable ?

  #include "newblue_bh1750.h"     I2C_HandleTypeDef *bh1750_i2c; // Handler to I2C interface   bh1750_mode Bh1750_Mode; // Current sensor mode uint8_t Bh1750_Mtreg; // Current MT register value   void BH1750_Init(I2C_HandleTypeDef *hi2c) { bh1...

0693W00000YAVmWQAX.png
MMARI.1 by Senior II
  • 2868 Views
  • 3 replies
  • 0 kudos

12 one time pulse timer ?

Hello !I need to create 12 (separately triggered pulse trains for thristors) one time pulse timers. (one pulse train consists of approx 10 pulses with approx 10us wide) Many stm32s only have 2 or 3 timers with RCR ( one pulse timer with repetition c...

OYoru.1 by Associate II
  • 1059 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.