STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Weird ADC failure STM32F091, any ideas

We've been building a PCB with four STM32F091s on each PCB and we've built about 50 units by now (over about 3 years). I have now seen three PCBs where the ADC readings are 'bad' on two of the four micros. By 'bad' I mean conversion values are 30% is...

ADC direct channel issue on STM32H7A3

Hello everyone,I'm having some throuble in reading the direct analog input on channel PA0_C.In my design I'm using several analog input. They seems to work properly in general and I have a precision more or less as expected. On channel PA0_C, though,...

0693W00000YAmL9QAL.png
MNico.2 by Associate II
  • 1507 Views
  • 1 replies
  • 0 kudos

Waking from Standby with any GPIO with STM32L4?

I thought of using an STM32 to build a device which responds to infrequent pushbutton presses, but should also conserve battery. My initial instinct was to use an STM32L4 in Standby or Shutdown mode, setting the GPIO as external interrupts which woul...

EPelt.1 by Associate II
  • 3302 Views
  • 2 replies
  • 0 kudos

STM32L162 LQFP64 device marking

Hi! We have received STM32L162 MCU in LQFP64 package with device marking that doesn't follow the datasheet. In the datasheet for this part product identification lines should be likeSTM32L162RDT6but on the part we had received it isSTM32L162RDT6So th...

AAGree by Associate II
  • 4201 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.