STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Why can I access 0x0810000 AXIM address in STM32F767ZG Flash , although the reference manual says that its only till 0x080F FFFF?

I am using STM32F767ZG for a project of mine. As per page 89 of the reference manual , it has 1 MB of flash and has a flash organization structure, as shown in the screenshot. The manual says that the "Main memory block" is limited to 0x080F FFFF. I ...

0693W00000aHLacQAG.png

Generate a pulse in the STM32H7 SPI's SS line every 64 bits

I want to communicate with an SPI slave whose high level protocol states that each command is 64 bits, and that the SS line must be de-asserted and asserted in between commands. I want to send to it 2 commands as quick as possible, so I need to asser...

0693W00000aHRfYQAW.png 0693W00000aHRglQAG.png
DGast.1 by Associate III
  • 1572 Views
  • 1 replies
  • 0 kudos

How to read Data with I2C from 3 Byte register?

Hello, I am new to STM32 so I am currently try get the basic done. I want to receive like written in the title, the temperature data from the BMP388 sensor. Therefore I looked up the Datasheet and found out that I need following registers.#define SLA...

Y-E-Quit by Associate
  • 3125 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F746IGT - Cannot trigger ADC conversion with Timer 4

Hello,I'm working on hobby project using STM32F746IGT. I wrote ADC init sequence but cannot get it working properly. Timer 4 reloads at given period and It's interrupt is called properly. ADC starts conversion after setting SWSTART bit manually but I...

RZieb by Associate II
  • 5833 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.