2021-06-28 1:32 PM
Hello,
I'm working on hobby project using STM32F746IGT. I wrote ADC init sequence but cannot get it working properly. Timer 4 reloads at given period and It's interrupt is called properly. ADC starts conversion after setting SWSTART bit manually but I cannot make Timer4 to trigger ADC1.
Please help :)
void adc_init( void )
{
RCC -> APB2ENR |= RCC_APB2ENR_ADC1EN;
RCC -> APB1ENR |= RCC_APB1ENR_TIM4EN;
RCC -> AHB1ENR |= RCC_AHB1ENR_GPIOAEN | RCC_AHB1ENR_GPIOHEN;
gpio_pin_cfg(GPIOA, 7, GPIO_ANALOG);
// Timer 4 TRGO
// Max 36 MHz @ 3.3V
ADC->CCR = ADC_CCR_ADCPRE_0 | ADC_CCR_ADCPRE_1;
ADC1->CR2 = ADC_CR2_EXTEN_0 | ADC_CR2_EXTSEL_3 | ADC_CR2_EXTSEL_2 | ADC_CR2_ADON;
ADC1->CR1 = ADC_CR1_SCAN | ADC_CR1_DISCEN | ADC_CR1_EOCIE;
ADC1->SQR1 = 0; // 1 regular conversion
ADC1->SQR3 = (7 << 0); // 1st conv IN7
ADC1->SMPR2 = (0b001 << (7*3)); // IN7 112 cycles
NVIC_EnableIRQ( ADC_IRQn );
NVIC_EnableIRQ( TIM4_IRQn );
ADC1->CR2 |= ADC_CR2_SWSTART;
// Sampling 16000 Hz
//
TIM4 -> ARR = 125 - 1;
// 500ns tick
//
TIM4 -> PSC = 216/2/2 - 1;
TIM4 -> CNT = 0;
TIM4 -> EGR = TIM_EGR_UG;
TIM4 -> CR2 = TIM_CR2_MMS_1;
TIM4 -> DIER = TIM_DIER_UIE;
TIM4 -> CR1 |= TIM_CR1_CEN;
}
void ADC_IRQHandler(void)
{
ADC1->SR = 0;
ADC->CSR = 0;
//static uint8_t val = 0;
double in = (double)(ADC1->DR-2048.0)/4096.0;
in++;
}
void TIM4_IRQHandler(void)
{
TIM4->SR = 0;
}
Solved! Go to Solution.
2021-06-29 1:36 AM
According to Erratasheet enabling DAC (!) clock is mandatory to get TRGO signal working:
RCC -> APB1ENR |= RCC_APB1ENR_DACEN;
It would be much easier for developers if they have placed that piece of information in ADC paragraph ;)
2021-06-28 2:50 PM
Looks OK.
SCAN and DISCEN are maybe redundant, but shouldn't make harm, similarly TIMx_DIER and clearing ADC_CSR (which is a read-only copy of the individual status registers).
Try to read out and check content of both TIM and ADC registers, maybe observing the status register(s).
JW
2021-06-28 10:51 PM
Thank you for your response.
Unfortunately every flag in registers seems OK. Probably there are some hardware issues with internal TRGO matrix.
RZ
2021-06-29 1:36 AM
According to Erratasheet enabling DAC (!) clock is mandatory to get TRGO signal working:
RCC -> APB1ENR |= RCC_APB1ENR_DACEN;
It would be much easier for developers if they have placed that piece of information in ADC paragraph ;)
2021-06-29 3:06 AM
Kudos for finding this.
Thanks for coming back with the answer. Please select your post as Best so that the thread is marked as Solved.
JW
2021-06-29 8:09 AM
What a bizarre requirement. Thanks for reporting. Sure enough, that's exactly what Cube examples do. Wonder if generated code would do the same as well.
2021-06-29 8:43 AM
> Sure enough, that's exactly what Cube examples do.
Oh, between steps 4 and 3 (in this order). Without a single line of explanation. Very characteristic.
JW
2021-06-29 8:49 AM
2021-06-29 9:18 AM
> Oh, between steps 4 and 3 (in this order). Without a single line of explanation. Very characteristic.
Indeed... What a mess...
2023-02-17 2:33 AM
> CubeMX generated code does not enable the DAC clock. I'm sure that will burn someone in the future.
It did.
@Amel NASRI , can you please have a look at this?
Thanks,
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.