STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! User external HSE on nucleo board bypass bit (HSEBYP) acts weird

Hi, I am trying to use an external frequency to drive my STM32F303RE, using a nucleo board (NUCLEO-F303RE). There is a lot of confusion going on right now. First of all, I was provided a nucleo board with an external oscillator that was already solde...

LT.1 by Associate II
  • 4393 Views
  • 3 replies
  • 0 kudos

Resolved! I2C Communication problem with STM32F103C8 Blue Pill Board.

I am using STM32F103C8 Blue Pill Board. I am trying to communicate with ATH20 Temperature & Humidity sensor from past One week. Configured STM32F103 Blue Pill - System Clock As (8mHz * PLL8 )= 64mHz and APB1 as 32mHz.I have Trouble wit START bit, Whe...

Siva Ram by Associate II
  • 4776 Views
  • 4 replies
  • 2 kudos

How to exactly reset Timer

In my project, I have to count exact time and I am using very sensitive external oscilator. I configure it as a external timer. I have a certain number of overflow counts and waste values for my count, when it reaches the waste value, I create a capt...

hdemi.1 by Associate III
  • 2489 Views
  • 3 replies
  • 0 kudos

Resolved! Where is ADCREF voltage set?

I use ADC 12 bit in STM32L03 and cannot find where CubeIDE defines which reference voltage the ADC should have. ADC_Init() is auto-generated. Is it the default used and what voltage is it?The processor is fed with 3.3V and has VDDA connected to that ...

Haddock by Associate III
  • 8037 Views
  • 10 replies
  • 0 kudos

Resolved! Timer interrupt not working in STM32G030x

We were using TIM16 to count and monitor if a button is pressed for more than 2 seconds. If pressed for more than 2 seconds, an interrupt will be generated and a flag will be set. This was successfully implemented when used as shown below:void HAL_TI...

0693W00000aHm2mQAC.png

STM32H7 Series: Shutdown/Low Power Mode High-Level Question

Hello,I am working with the STM32H7B3IIT6 MCU and it is controlling many features (CANbus, BLE, LCD Display, push buttons, etc.). One feature we're going to have on our system, naturally, is a simple on/off button that powers the overall system on an...

KMew by Senior III
  • 8954 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.