2023-03-04 2:26 PM
2023-03-05 3:03 AM
no. why ?
2023-03-05 12:27 PM
Because in some sections of my application I want the dac to output continuous waveforms from a lookup table and in other sections I want it to output a single pass of a lookup table in response to an event. What I now have found to work is:
((DMA_Stream_TypeDef *)hdma_dacX_chx.Instance)->CR |= 0x100;
For continuous output, bit 8 set selects continuous and
((DMA_Stream_TypeDef *)hdma_dacX_chx.Instance)->CR |= ~0x100;
For one shot output, bit 8 reset selects normal, X is the dac and x is the channel.
The reference manual indicates the bit 8 information but getting to it using HAL definitions required some investigation.
2023-03-05 3:24 PM
>((DMA_Stream_TypeDef *)hdma_dacX_chx.Instance)->CR |= ~0x100;
No. &=.
JW
2023-03-06 5:45 AM
Yes, my bad.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.