STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error in PM0214 Programming manual with "vmla" instuction?

I think there is an error in the PM0214 Programming manual "STM32 Cortex® -M4 MCUs and MPUs programming manual". The multiply and accumulate instruction is called "vlma" throuout the whole document. Other programmin manuals (e.g. for STM32H7) as well...

herbert by Associate III
  • 2062 Views
  • 2 replies
  • 1 kudos

How to output two DACs through stm32?

I have a STM32-G071RB. I want to generate two sine outputs. one for reference and the second with a phase shift. Unfortunately, there is only one DAC port. I got an extra board but then I realized I need communication between the two boards to (I fou...

RShre.2 by Associate III
  • 3734 Views
  • 6 replies
  • 0 kudos

UART communication problem. No reception

HelloI am trying to communicate with a Daly BMS in UART. I tried at first with an arduino board where I got the desired frame but when I tried with a custom made STM32F072 board. But during this test I can't get any response from the BMS.The BMS work...

bvale.2 by Associate II
  • 5188 Views
  • 8 replies
  • 0 kudos

Resolved! Error in reference manual of STM32G4

I think there is an error in the reference manual (RM0440 Rev 7) in chapter 24.5 - COMP interrupts.At the end of this chapter it says: "Interrupt events are flagged through COMP_CxCSR flags."But in COMP_CxCSR register there is no flag for interrupt e...

Moritz1 by Associate III
  • 2422 Views
  • 4 replies
  • 0 kudos

Schematic for Nucleo STM32F072 has unconnected jumpers.

I've noticed that the Nucleo STM32F072 has two jumpers (CN11 and CN12) that connect ground to ground. Does anyone know why this is? Are these jumpers used on another Nucleo board, and just hang out on the STM32F072 like a lot of the unconnected sol...

EThay.1 by Associate
  • 2017 Views
  • 3 replies
  • 0 kudos

STM32 MCU UART TX current

I am connecting the STM32L4 MCU UART to silicon labs IC CP2105 (UART to USB converter). The UART to USB bridge is bus powered from the type C connector and the STM32 is separately powered from the battery. When the CP2105 is in off state ( No USB ca...

KK.4 by Associate II
  • 1640 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.