STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Does PVD work in Stop mode?

STM32L072CZTxPVD is configured to trigger INT16 and wake up the MCU.It is working with the MCU in Sleep mode.However, when the MCU is in Stop mode the interrupt does not trigger.After reading RM0376 I am unsure if PVD is supposed to work in Stop mode...

helioz by Associate II
  • 1716 Views
  • 2 replies
  • 0 kudos

PC13 disturbs LSE erratum is widespread

Trying to answer https://community.st.com/s/question/0D53W00002HBKtaSAH/stm32l452-lse-pc13-errata I realized it's a widespread erratum which recently appeared in most older STM32 errata.I understand that issues like these may surface after years. OTO...

Resolved! Repeated Start bit code without memory address

I am using a Flintec TR2 board, and I want to communicate with it via my STM32 L496zg Nucleo Board. It uses I2C repeated start condition to communicate. Most of the codes I found online suggest using HAL_I2C_Mem_Read/Write functions but the user manu...

AVima.1 by Associate
  • 1557 Views
  • 2 replies
  • 0 kudos

STM32F745 - Disable Watchdog in Sleep mode

Hello,I am using STM32F745VEHx. I would like to disable the software independent watchdog before microcontroller goes into Sleep low power mode and then re-enable it once microcontroller comes out of Sleep. I can find literature which suggests this c...

LJain.1 by Associate II
  • 1361 Views
  • 1 replies
  • 0 kudos

STM32F303K8 - Sampling a 40KHz sine-wave

The problemI am to compare the phase shift between two sinewaves from an external source (I used a function generator in this case). I am running the STM32F303K8 at 64MHz, and this clock goes directly to the ADC and Timers 1 and 2 as well with a pres...

_legacyfs_online_stmicro_images_0693W00000bku8LQAQ.png _legacyfs_online_stmicro_images_0693W00000bku8kQAA.png
malehakim by Associate III
  • 4366 Views
  • 3 replies
  • 0 kudos

Resolved! stm32f334 i2c slave speed

Stm32f334 i2c works in slave mode , select i2c kernel clock 72mhz. datasheet says it's i2c fast-mode+ support up to 1mhz, but I found that it can be accessed stably by a master with scl at 2.5mhz. Is it ok to use a master scl speed faster than...

tri.1 by Associate
  • 2412 Views
  • 1 replies
  • 0 kudos

STM32F429 SD card rcvr_datablock time

I have a application with STM32F429ZI and SD card withour RTOS.I have a llong time for write in a SD card.The rcvr_datablock routine is loong about 3 ms between set and reset LED !!!It is possible to reduce this time using rot_rdq without use a RTOS ...

IlConte by Associate III
  • 891 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.