STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Linker handles TFlite differently on different boards

I have two boards: STM32L4xx and STM32H7xxQ.I use cubeAI 8.0.1 and tflite for a project in vision.Having set all includes and settings, I successfully build and flash my code on the first board. The second project uses the same include paths (exporte...

KZait.1 by Associate
  • 818 Views
  • 0 replies
  • 0 kudos

Timer cookbook wrong figure ?

Shortly, cookbook says ETR frequency higher than core clock. It seems wrong. I am not sure if the information given is correct.

_legacyfs_online_stmicro_images_0693W00000dJtpXQAS.png
hdemi.1 by Associate III
  • 2600 Views
  • 4 replies
  • 0 kudos

Stm32F4 i2c as master trasmit HAL_OK but not working

I’m using the board, motordriver IIC, to control motor through I2C bus.The chip on the board is PCA9685.​The board is originally a extension for arduino UNO, and I’m using STM32F446RE which also support arduino UNO expansion connector.​The official g...

0693W00000bhIjYQAU.png 0693W00000bhInFQAU.png 0693W00000bhIrbQAE.png 0693W00000bhIsPQAU.png
JChen.43 by Associate II
  • 5441 Views
  • 11 replies
  • 0 kudos

Resolved! STM32H7 Option bytes programming halts CPU

The MCU halts for approximately 300ms after setting the OPTSTART bit in the FLASH_OPTCR register. In HAL_FLASH_OB_Launch() :HAL_StatusTypeDef HAL_FLASH_OB_Launch(void) { HAL_StatusTypeDef status;   /* Wait for CRC computation to be completed */ ...

NilocA by Associate
  • 1571 Views
  • 2 replies
  • 0 kudos

How to connect to U5 discovery board on Windows 11

Hello,​I have watched the ST video "Discover the new STM32U5 IoT node B-U585-IOT02A Discovery kit", which showed using the STLink Virtual COM Port (VCP) with a terminal program to connect to the board. I've also seen articles, with no answers, about ...

EC.3 by Associate III
  • 1261 Views
  • 1 replies
  • 0 kudos

STM32L5 - Single Bank Flash Mode

I'm attempting to switch to single-bank flash mode on an STM32L562ZET6Q (512k Flash), but so far I've been unable to get the Flash OPTR to operate as the reference manual claims.I used the normal process for modifying the OPTR: HAL_FLASH_Unloc...

MBand.3 by Associate III
  • 5729 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.