STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Trigger HRTIM capture via SW (i.e. EXTI event)

I use the HAL to setup multiple HRTIM timers on a STM32G4 and I would like to trigger a simultaneous capture across them using software (the reasons for this are complex but it needs to be a simultaneous capture).Currently I have a GPIO output pin lo...

g mcclean by Associate II
  • 1780 Views
  • 2 replies
  • 0 kudos

Hi, I've purchased an STM32H723ZG Nucleo Board to evaluate and test the potential of the onboard DAC. The max sampling time for the STM32H72x with the max bus speed at 137.5MHz is 51.1Msps as described in the AN4566 but I can't reach them.

I'm trying to generate a 1.2 MHz sine burst using the DAC, DMA and Timers. Everything works fine but only up to 200-250KHz then increasing the frequency the amplitude begins to decrease.Moreover I've managed to reach about 25Msps and it seems impossi...

MZ.NG by Associate
  • 1642 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H747IGT6 Flash read leading to hardfault

Hi,We have written the data in Flash Bank 2 sector 7 successfully. Power cycled the board and trying to read the stored data from Flash Bank 2 sector 7 and found Hadrdfault error at 64th byte.-> The data stored in the form of char.-> Using HAL librar...

_legacyfs_online_stmicro_images_0693W00000dDOhuQAG.png
SH.3 by Associate
  • 4862 Views
  • 1 replies
  • 0 kudos

How to receive data by using SPI communication ?

I use the STM32Lo538 disco board, and this board is connected to one sensor. Moreover, the protocol of this sensor is SPI. I faced difficulties receiving the data from the sensor. When I watched the waveform of this sensor, I noticed that the CS pin ...

Timer Encoder

Hi, I am using STM32F105 MCU.I have made a mistake in Hardware and switched two pins around. I have two signals from a encoder which they are connected to MCU in wrong way. SignalA ---> PC9 (TIM3-CH4)SignalB ---> PA8 (TIM1-CH1)I want to use a combin...

NASI by Senior
  • 1565 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.