STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C Problem

I have 2 MCU, one is the STM32F401RE acting as master and the other is STM32G474RE acting as slave, I have kept both the controllers in open drain and pulled up, the slave address is 0x30<<1, I think the data is being transferred because on pressing ...

Epsilon03 by Associate II
  • 2967 Views
  • 4 replies
  • 0 kudos

How to map STM32G0B0 DMA to UART1 TX

STM32CubeIDE Version: 1.12.0Using LL driversADC to Memory via DMA1 Channel1 workingUSART1 RX worksMemory to USART1 TX via DMA1 Channel2 does not work     I'm guessing the problem we are having is that we are not using the correct DMA channel for USAR...

Resolved! STM32L4 HAL I2C driver not working anymore after update

I recently update my STM32L4 HAL library from 1.9 to 1.13.  After that, using the HAL_I2C_Mem_Write_IT function, I got stuck in an error routine because TCR flag was set and that shouldn't happen:        When I looked at the changes in the HAL librar...

Schermafbeelding 2023-07-02 om 17.08.20.png Schermafbeelding 2023-07-02 om 17.06.53.png

Receive into external RAM via DMCI

uC: STM32H725AEIToolchain / IDE: STM32CubeIDECubeMX version: 6.8.0I'm using CubeMX for code generation with HAL drivers.I'm currenty receiving a JPEG from a camera via DCMI with 640x480.I'd like to step up the game to 1280x960, but the picture would ...

STM32F4 two PWM pulses with different lengths by using DMA

Good evening ST experts, I hope that some of you can help me with my problem.As the titel already states, I am trying to generate two pulses with different lengths (same length, but different CCRs) by using a DMA timer function:HAL_TIM_PWM_Start_DMA(...

SCR-20230703-twzs.png
AAnge.3 by Associate
  • 1671 Views
  • 2 replies
  • 0 kudos

Resolved! STM34L431 UART receive on Pin PB10, Pin always high signal

Hello,I have a problem with the Controller. For some time the Uart is working fine. Than the UART receive Interrupt is not generated anymore.I check the working pcb with the debugger and the scope. I see there is no Signal on the pin. The uart from t...

M.Harms by Associate II
  • 6552 Views
  • 6 replies
  • 0 kudos

STM32H743XI silicon Y - DBGMCU dead ?

Curious if anyone else encountered this: I work on a design using STM32H743XI silicon Y and DBGMCU seems to be completely dead. Reading any register returns 0 (so no REV_ID/DEV_ID). Writing to get 'timer freeze on debug' does not work either and read...

Dan4 by Associate II
  • 10398 Views
  • 22 replies
  • 0 kudos

STM32H562 DMA_LINKLIST on ADC

We are testing the latest STM32H562RGT device on our application. I am running an eight-channel ADC (on ADC1) with DMA support. All eight channels gets populated with the correct ADC values, however, the DMA InitLinkList State stays on BUSY and thus ...

LeRoux by Associate
  • 1435 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.