STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 SDIO CLK line is running below 400 kHz

Hello,    I have a really strange problem with our STMF407 custom board that connects to a full-size SD Card socket using SDIO.  The MCU uses HSE at 8MHz and SDIO configuration as a 4-bit wide bus and div factor = 0.  All the other values are SDIO de...

PChao.2 by Associate II
  • 3482 Views
  • 2 replies
  • 1 kudos

LCD MB1166-A09 and LCD MB1166-A03

Hi, We had an LCD problem with a recently bought board STM32F769I-DISCO, revision MB1166-A09. Now it's resolved by recompilation with macro "USE_STM32F769I_DISCO_REVB03" entered in project options. My question now is how can I make it universal, with...

DShub.1 by Associate II
  • 2894 Views
  • 2 replies
  • 0 kudos

STM32F730R8T6

ST states that the STM32F730R8T6 has Quad SPI, but it is missing QUADSPI_BK1_IO2 on the pinout?!?!  

BBrow.2 by Associate III
  • 1466 Views
  • 2 replies
  • 0 kudos

Resolved! EP0 IN transfer times out

For learning (and suffering) purposes I am trying to write my own USB Driver in device mode. Right now I am just trying to successfully enumerate the device. So far I am able to read SETUP packets but when writing to EP0 (IN transfer) the requests se...

rudbeckia by Associate II
  • 6364 Views
  • 7 replies
  • 0 kudos

QSPI unexpected clock behavior STM32H723VGTx

Dear Community,for my application I use the STM32H723VGTx where I'm using the OSPI interface as a SPI and QSPI to control a external sensor (MCU SPI master, sensor SPI slave). Now I face some issues with this communication interface, for debugging re...

Screenshot_20230710_061705.png Screenshot_20230710_063602.png Screenshot_20230710_061552.png

Uploading option bytes over DFU

Hi, I have a custom board using STM32G431CBU6. I am using `dfu-util` to upload firmware and option bytes. I don't have any problem reading/writing flash area with DFU, and I can read the Option Bytes area with DFU, but when I try to upload a valid op...

USB not working in hard fault handler

I am trying to dump stack trace from hard fault handler using usb, but the usb not working in hardfault handler.Any one please help me to know why usb not working in  hard fault handler, if there is a way to use usb in hard fault handler

Anand m by Associate II
  • 4632 Views
  • 8 replies
  • 4 kudos

variable phase shift between two PWM signals

Hi,I am trying to create to PWM outputs with a variable phase shift between them. They are of fixed frequency, 50% duty and exactly the same shape but with variable phase shift. I need to dynamically change the phase shift between them as a control p...

mosiTX by Associate
  • 1800 Views
  • 2 replies
  • 1 kudos

STM32G051F8P6 GPIO state during reset

Hello,I have some strange behavior with a circuit.  My understanding is that the GPIO should be configured as an input at power up, however, I am seeing a brief flash on an LED during power up and Power down (images attached showing circuit and the 3...

troper by Associate
  • 1888 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.