STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

External Loader Algorithm with LTDC Initial Failded

Hi,I`m using small internal flash MCU for my research, so I need to store all function and data on external flash.The File Extension is called *.stldr that generated from External Loader Algorithm. After programming, all function works fine.Now I con...

Resolved! Debugging with the STM32F205RCT6 not working

Hi, i'm realative new to using ST products and i'm currently trying to debug with the STM32F205RCT6 using the ST-LINK V2 with the debug protocol SWD. but it's simply not worinking, it keeps saying No device found on target.  This is how it's connecte...

Screenshot_152.png Screenshot_154.png photo_2023-08-08_23-26-07.jpg

Resolved! TIM5 accuracy and overflow: configuration

I am trying to configure the TIM5 to get timestamp in milliseconds for a long period (over 40 seconds).Here is the current configuration of TIM5:// This function inits and start the timers usedvoid timer_init(void) { __HAL_RCC_TIM5_CLK_ENABLE(); ...

STM32U5 STLINK compatibility

Hello. We are building a widget using the new STM32U5 (BGA) device. So far, so good. Need to have an onboard STLINK 2.1 with drag & drop feature to allow for easy to use end user firmware upgrades. Could someone please confirm that the STLINK v2.1 is...

Mon2 by Senior III
  • 1739 Views
  • 1 replies
  • 0 kudos

MTBF of STM32F446xC/E

I am looking for MTBF of  STM32F446xC/E. Kindly share the Reliability/MTBF of  STM32F446xC/E if available. @STM32F446xC/E, 

Dheeraj by Associate
  • 1544 Views
  • 2 replies
  • 0 kudos

USART1 working but USART2 and USART3 no

Hi!I am working on a project where multiple sensors are connected to the stm32f4 transmistting data on a very high baud rate and then the received data is transmitted through USB VCP. For these matters I used DMA with USART1, USART2 and USART3 and im...

LOnGr.1 by Associate III
  • 1521 Views
  • 1 replies
  • 0 kudos

STM32L010K4 code protection

Hello All,I want to protect my code from reading by strangers using STM programmers. But I also I do not want to protect EEPROM. Because I am downloading Software verison and revision info to EEPROM incase I need to re-program IC.I am using STM32L010...

dc_stm by Associate
  • 2549 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.