STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Regarding the COM PORT not showing

I was getting Start with STM32F401CCU. I am not able to find the COM PORT to USE in ARDUINO IDE.But in Device Manager i was able to find the belowAs STM32 BootLoader. Which i am not able use ARDUINO IDE.Can AnyBody help me to fix this

AkarshSM_0-1691862376322.png AkarshSM_1-1691862433004.png

stm32 h747 uart8 hal_uart_init wrong

If when i use hal_uart_init(&huart8) get result Details:HAL_ERROR Default:HAL_ERROR,Decimal:1,Hex:0x1,Binary:1,Octal:01.When i use step into ,reach at final while(sets-- !=0u)and no more what does this mean ? how could i solve this problem? static vo...

wjian2_0-1691841082867.png
wjian.2 by Associate III
  • 1760 Views
  • 3 replies
  • 0 kudos

STM32H563 and STM32CubeIDE

For Debug Pinout and Configuration I see External Trigger Bi-directional associated with PC7. What is this? What are the voltage levels?

Several DMA streams running in "parallel"

Hello!I'm new to DMA concept, and need some clarification on several DMA questions (STM32h7). Q1. From RM0433: "To ensure data coherence, each group of transfers that form a burst are indivisible: AHB transfers are locked and the arbiter of the AHB b...

MNema.1 by Associate III
  • 1769 Views
  • 2 replies
  • 0 kudos

Trigering ADC in the Middle of PWM ON Duty Cycle

Posted on February 07, 2013 at 19:23Hello, My intention is using TIM1 Complementary PWM Channel 1-3 for Brushless Motor Control. I want to sample the Phase Voltage at the middle of PWM ON Duty Cycle. I have configure TIM1 to output 6 Channel PWM but...

Resolved! STM32H563VI Octo-SPI interface dummy cycles

Hi,someone can explain me how to calculate the "dummy cycles" number reading an external flash qspi such as the Winbond W25Q64JV ?I have to read in qspi mode with the Fast Read Quad I/O (EBh) command in SDR mode. The flash memory datasheet asks for 4...

Ez by Associate II
  • 6398 Views
  • 4 replies
  • 1 kudos

Resolved! Efficient de-interleaving without waking the CPU

I am using the STM32G474 and have the following situation:I have configured a Timer to run continuously at 25 kHzThe Timer triggers the ADC to start a sequence of 6 conversions (i.e. 6 ADC channels)Upon completion of each ADC conversion, DMA transfer...

Olly by Associate II
  • 3609 Views
  • 5 replies
  • 4 kudos

Resolved! Unable to get maximum SYSCLK of 480MHz on STM32H743XIH

With SYSCLK set to 400MHz in MX Clock Configuration there is no problem, but any setting above ~420 up to the maximum of 480Mhz causes the system to 'crash' during initialisation in HAL_RCC_ClockConfig(..). More specifically when or after RCC->CFGR i...

DavidO by Associate II
  • 3074 Views
  • 4 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.