STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Jump to user application using OpenBootloader on STM32G4

Hi Community,I recently started working on OpenBootloader on a NUCLEO-G491RE and was trying to understand its operation. As an initial step to understanding the protocol and operation used a terminal and sent commands manually those can be found in t...

Resolved! Should I solder and unsolder on the X-NUCLEO-CCA01M1 and X-NUCLEO-CCA02M2 for the Acoustic Echo Cancelling function package ?

I am trying to set-up the demo-kit for Acoustic Echo Cancelling and I am a bit confused about steps 1 and 2 of Getting started with the STM32Cube function pack for acoustic echo cancellation - User manual in part 2.3.1.On my boards bridges that shoul...

MMarn.1 by Associate
  • 2078 Views
  • 3 replies
  • 1 kudos

Resolved! USART-5 on STM32 LoRa

HiWe are using the DISCO-L072CZ-LRWAN1.USART-5 uses pin PB3 for Tx, is this pin not available on the LoRa development kit ?Is there a way to re-route the USART-5 Tx pin or access it ?thanks

sgabran by Associate III
  • 2346 Views
  • 2 replies
  • 3 kudos

Resolved! Stm32h747-Disco uart to arduino

UM2411:Caution: The I/Os of the STM32 microcontroller are +3V3 compatible instead of 5 V for ARDUINO ®Uno V3This mean can not conect to Stm32h747-Disco with pines for uart to arduino directly o no ? If hay problem with this how to send data o solve t...

wjian.2 by Associate III
  • 1574 Views
  • 1 replies
  • 0 kudos

Resolved! Finding/Porting Examples?

Hello, I have the STM32G474 Discovery Kit and am just attempting to get a blinky LED program to work on it for right now. In the STM32CubeIDE, I imported an example, was able to get it to build correctly (after changing references from caddr_t to voi...

5555.png
ewilliams by Associate II
  • 1954 Views
  • 2 replies
  • 0 kudos

Resolved! HAL and GPIO EXTI

If I register a callback function for GPIO EXTI and I have EXTI on multiple ports for the same pin (e.g. PA0 and PB0) how does the callback distinguish between the ports when the event triggers?

Resolved! Timer interrupting on MCU reset

Hello I have set the timer7 for 1 minute interrupt. It is working at every minute as expected. But the interrupt is also triggered as MCU is reset. I have set global counter for increment in timer7 callback. As soon MCU is reset , Timer7 callback is ...

Nico3 by Senior
  • 2357 Views
  • 2 replies
  • 1 kudos

Resolved! PLL clock division in STM32H7 for fadc_ker_ck

Hi,a footnote(4) in STM32H7 reference manual RM0468 Table 56 regarding the maximum allowed frequency for ADC says"With a duty cycle close to 50%, meaning that DIV[P/Q/R]x values shall be even".Does this recommendation apply to the actual DIVXx regist...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.