STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

master full spi register with stm32l010c6t6

Hi everyone! i am work with stm32l010c6t6 for comunicate llcc68 Lora module using spi, i find the standard peripheral library and not have, i don´t want use hal because i need maior control. i am using the example but this is using stm32f103c8t6 and ...

jdo by Associate II
  • 955 Views
  • 0 replies
  • 0 kudos

Resolved! HAL_UART_Receive_IT() only fires once, and I don't know why.

Hi!I am trying to write a program where I am waiting for receiving 6 bytes of data through UART. It works just fine the first time, than I restart the receive_IT function and nothing happens anymore. I have other codes where I use it just the same, t...

BBara.1 by Associate II
  • 12969 Views
  • 11 replies
  • 2 kudos

Where to find DFU examples?

Hello, I have both the B-G474E-DPOW1 and the STM32F407G-DISC1.According to the AN3156 I saw that both the G4 and F4 series support DFU. I wanted to demo this capability with either of these boards, but I can't find any examples specific to these targ...

ewilliams by Associate II
  • 1370 Views
  • 1 replies
  • 0 kudos

NUCLEO-PGEEZ1 on STM32L4R5

Hi,my problem is somehow close to this post "How to run NUCLEO-PGEEZ1 on NUCLEO-L476RG board? " So, I have followed the structure for my board STM32L4R5 IT6 and I don't have error in my program.My problem is, I can't get  my expected result from EEPR...

Screenshot Result.png app_x-cube-eeprma1.png LogicAnalyzer.png
N.goli by Associate
  • 778 Views
  • 0 replies
  • 0 kudos

Lift monitoring using STM32WLE5 (RAK3172)

Hello and thank you for your time :)This post is about recommendations or best practice ideas, and first, I will introduce my project.As the title states, the goal is to create a "lift monitoring" device using the STM32WLE5.The device should detect a...

Dodo by Associate II
  • 1926 Views
  • 1 replies
  • 0 kudos

FDCAN fail to run with OTA firmware

Hi there! I am writing to bring to your attention an issue we have encountered during the testing phase of the firmware for the STM32G474VET6-based microcontroller. The core of the problem revolves around the functionality of the FDCAN interface when...

Query regarding Power Up of STUSB4500

I was working on a project of power delivery using STUSB4500. I am configuring the STUSB4500 registers using a Nucleo F07. So, my query is whether we can connect the Nucleo Board for UART / I2C Connection and the Type C Power Adapter for Source Input...

b.png
theAkash by Associate
  • 1224 Views
  • 0 replies
  • 0 kudos

Resolved! Unable to write to register (example ADC1->SMPR = 7)

I am trying to use the AD converter on my Nucleo-F030R8 board. (Actually it works with the "HAL" functions, but I am trying to program on a lower level).While debugging I am watching my struct ADC1 (Wich points at the ADC registers). I am trying to w...

RBakk.2 by Associate
  • 1220 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.