STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32h725 doesn't work.

Hello, I looked at AN5419 and configured the stm32H725igk6 power supply circuit as shown in the following figure, but the external osc does not work and the st link is not connected to the MCU. Is this product a model that must be configured using S...

sangmin_0-1691549389868.png
sangmin by Associate II
  • 8621 Views
  • 9 replies
  • 9 kudos

STM32U575ZI Configuring ADC1 with GPDMA (without Linked List)

Hi !I'm trying to configure the ADC1 to 7 ranks conversion and a GPDMA1 channel (0) in "Standard Request Mode" to transfer the ADC data into the memory.First, I've configured the ADC without GPDMA channel, and it worked fine (Polling mode, no interru...

TTaie.1 by Associate II
  • 3198 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 FLASH Write Protection Error

Hi there!I was trying to emulate eeprom using flash memory. I am using Nucleo-F030R8 board. I was able to program flash 2 times (0xF055 was the test value):however I cannot reproduce it anymore and whilst trying to program I get PGERR.Uploading my co...

Jouls_1-1692196000827.png
Jouls by Associate II
  • 3705 Views
  • 3 replies
  • 3 kudos

Resolved! TIMER interrupt priority using Register in STM32G030K6T6

i am Initialize  UART2 and timer1 then my timer interrupt and UART2 interrupt in working fine but when i set priority timer first they do not set why? void main(void){NVIC-Set-Priority(TIM1_BRK_UP_TRG_COM_IRQn, 0);NVIC-Enable-IRQ(TIM1_BRK_UP_TRG_COM_...

UART Receive Interrupt update global variables

Using UART in Receiving Interrupt mode, I want to update various global variables values from console like Putty.  Something like first send the opcode and then value. Please suggest if any sample codes available. I am relatively new to programming w...

Nico3 by Senior
  • 1118 Views
  • 1 replies
  • 0 kudos

SDRAM signals - FMC_NL and FMC_SDNWAIT

Using STM32H743IGKx.Tools: LinuxSTM32CubeIDEVersion: 1.12.1Build: 16088_20230420_1057 (UTC)STMCubeMXVersion: 6.8.1-RC4Build: 20230419-1431 (UTC)When setting up the SDRAM configuration in MX, I end up with a couple of signals that look like they are n...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.