STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

No device found on target

I can't seem to connect to my STM32F401RCT6. This is the schematic below and all the jumper wires are working. Can anyone spot the error?When i try to connect to it i get the message 'No device found on target' 

Hesseltjuuh_0-1692368912118.png

[STM32H745XI-DISCO] Unable to debug CM4

Hi community,I'm trying to launch an ANN on this discovery board.I build and programm both CM without error.However I'm not able to debug CM4 and have this error :Starting server with the following options:    Persistent Mode      : Disabled    Loggi...

BKOSI.1 by Associate II
  • 5703 Views
  • 9 replies
  • 0 kudos

Resolved! ST-Link starts firmware and aborts it while downloading

Hello,I am using STM32CubeIDe V1.10.0.my project is structured as follows:-CubeMX inits-HAL_I2C_IsDeviceReady-HAL_I2C_Mem_Read //Read a large amount from an I2C EEPROM-while(1)I have now done a lot of troubleshooting to understand why HAL_I2C_IsDevic...

mfrank9 by Associate III
  • 3668 Views
  • 6 replies
  • 2 kudos

STM32 HAL driver for SST26VF064B

Posted on June 23, 2018 at 23:02I just start to create a driver for SST26VF064B Serial Flash in QSPI mode.Anyone knows where I may able to get an example using the HAL layer QSPI driver ?

Resolved! Problem with STM32L0538 - Discovery

Hi,I have an STM32L0538 discovery board and I'm trying the Demo example. The problem is that it does not work. When I flash the board it changes the e-ink display like this:Also when I touch the bottom bar it does nothing. The revision of the board i...

photo_2023-08-15_20-43-26.jpg Captura de pantalla de 2023-08-15 20-47-46.png
BTurc.2 by Senior
  • 4142 Views
  • 9 replies
  • 5 kudos

Programming manual document may need list of requirements

A novice HAL programmer responded with this image:I did not find any extended information on the HAL_I2C_Master_Transmit function.There are a lot of incorrect codes on the Internet with this function, there are even videos on YouTube with the incorre...

PM_req.png PM_REQ2.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.