STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL Library for Medical device EN62304

Hello Everyone I dont know if its the correct place to ask . We design a medical device where EN62304 calss C is applied . the standart says if we use an 3rd party software ( any library ) should be designed to use for medical devices. What about HAL...

STM32L476 SPI incorrect readings

I am trying to communicate with a spectrometer sensor using SPI protocol. With SPI default settings, I am using both arduino and Stm32L476 nucleo boards. (8Bits, MSB First, CPOL Low, CPHA 1 Edge).I read multiple registers from the sensor using both a...

RSath.1 by Associate II
  • 4139 Views
  • 5 replies
  • 0 kudos

HAL_GPIO_TogglePin() not thread-safe

Posted on May 30, 2018 at 21:31STM32Cube_FW_F7_V1.11.0's HAL_GPIO_TogglePin() appears broken in a multi-threaded environment:void HAL_GPIO_TogglePin(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin){  /* Check the parameters */  assert_param(IS_GPIO_PIN(GPIO_...

Resolved! How to efficiently save and restore the 32F407 FPU context

STM should really post their code to handle FPU context saving and restoring BECAUSE their clients have been asking for over a decade!!!One user stated "the time for a full FPU state save/restore is quite long. A pair of vpush {s0-31}/vpop {s0-s31} t...

Robmar by Senior III
  • 7257 Views
  • 12 replies
  • 0 kudos

Resolved! STM32 Product Recommendation

Among STM32 boards, I would like to recommend a board that includes an interrupt 2 or more pins, I/O (Analog) 20 or more pins, MCLR (reset), PWM signal (more than 2 pins), AVdd, AVss, Vss, RX, TX, ICDCLK, and ICDDATA pins. This is the first board I'm...

Park by Associate II
  • 2894 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H7: UART IDLE is set again without RXFNE be set.

I have the problem on my STM32H753, that the IDLE-bit is set when transmitting. On the manual it says: The IDLE bit is not set again until the RXFNE bit has been set (i.e. a new idle line occurs).The RXFNE is never set (actually on CubeIDE this is sh...

jhi by Senior
  • 3406 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.