STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 problem with UART Rx IT callback

Hello everyone!After many hours of grinding through forums & discussing with ChatGPT (really, ChatGPT is like my best friend now), I still fail to understand what must be a simple notion with an easy solution. This is why I'm posting this in forums. ...

CAdat.1 by Associate II
  • 8950 Views
  • 5 replies
  • 0 kudos

Resolved! STM32U5 with MX25R6435F is madness ?

Hi,This is driving me crazy, let me explain.Setup : NucleoU575 with MX25R6435F in QSPI with wire jumper cables. Here's a code adapted from an ST example for the stm32l496g_discovery.The modifications were minor, and we simplified it to the maximum, j...

Bertha by Associate III
  • 10106 Views
  • 13 replies
  • 5 kudos

NUCLEO-H723ZG ADC Accuracy Problem

HeyI have a few question about working with the ADC on NUCLEO-H723ZG (The mcu is STM32H7237ZG)1.I try to work with the ADC, I saw some example in the internet and I tried to use this examples.This is the function that I tried:HAL_ADC_Start(&hadc1); /...

TOsso.1 by Associate III
  • 1334 Views
  • 1 replies
  • 0 kudos

STM32f765 USB OTG

Hello, I see this in Errata es0334-stm32f76xxx."Host packet transmission may hang when connecting through a hub to a low-speed device"When the USB on-the-go full-speed peripheral connects to a low-speed device via a hub, the transmitter internalstate...

Shinoy by Associate II
  • 1329 Views
  • 1 replies
  • 0 kudos

STM32H753 vs STM32H23 radiation tolerance

We plan to use a STM32H723 for our main MCU on board a student CubeSat.We are currently verifying if this is a feasible option. I came across this report by the Open Source Satellite Project testing radiation effects on the STM32H753.As they are from...

ka1 by Associate
  • 3179 Views
  • 1 replies
  • 1 kudos

STM23L412 Flash Erase and Programming (EEPROM Emulation) Issue

I'm trying to write a code to store some values at the final flash page (no. 63) of STM32L412 I succeeded into erasing the page, but I'm failing to write anything to it, the code is based on the reference manual (RM0394)https://www.st.com/resource/en...

Mkotb by Associate II
  • 4606 Views
  • 4 replies
  • 0 kudos

convert 10-bit data uint10_t to float

i m using STM32H7 SPI to interface to external 10-bit ADC, which return a 16-bit data but only the last 10 bit (from LSB) is valid. How can i convert this 10-bit data to float ? and how can i obtain these 10-bit from the 16 bit data, i know i would n...

Keeping 2 Timer Interrupts with different Frequencies in Sync

Hello,I have two 32bit timers running on an STM32F373, TIM2 and TIM5.  I have successfully chosen TIM2's prescale and ARR values to generate the 'update' interrupt as I require by using TIM2's prescale set to 0 and modifying the ARR to set  a target ...

LMorr.3 by Senior II
  • 2171 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.