2023-10-05 2:45 AM - edited 2023-10-05 2:45 AM
We plan to use a STM32H723 for our main MCU on board a student CubeSat.
We are currently verifying if this is a feasible option. I came across this report by the Open Source Satellite Project testing radiation effects on the STM32H753.
As they are from the same series but not the same line of MCUs I was wondering if the report is roughly applicable also to the STM32H723 used by us.
I would be glad to head it if anybody had some input regarding this topic.
Thanks in advance
Kai
2023-11-11 6:07 AM
Dear @ka1,
We confirm that both MCUs are based on same Technology Node and libraries which is a proprietary STMicroelectronics 40nm Process - immunity versus radiation and alpha particles as the same , with the difference that STM32H723 has a smaller silicon size and less digital So I’m expecting function operations improvements versus the great 2021 Report from OpenSatellite org .
Cheers,
STOne-32
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.