STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L4xx TAMP/BKP register use problems

Greetings,I'm attempting to make use of the tamper backup registers.I am enabling the RTC and have using LSI as the clock source.ROP is not enabled, I am not using the TAMP input pins, and i am debugging via SWD.As it is at the moment, writing a valu...

mwp by Senior
  • 4143 Views
  • 9 replies
  • 3 kudos

Resolved! Microcontroller getting damaged when connecting to a VCU

I am using STM32G0c8t6 microcontroller to make a BLDC motor controller. I am connecting the Rx and Tx of UART to a VCU and they are sharing the same battery. Apart from these, there is no other connection between them. And sometimes, for some unknown...

Untitled (1).png
Gladson by Associate III
  • 3937 Views
  • 7 replies
  • 3 kudos

flashing error

Hi Team i am facing some issue related to flashing code. previously i flashed the STM32Cube_FW_WL Lora wan example code into my stm32wl5cc controller PCB using J-link debugger. after successfully flashed the code i am trying to flash another code int...

kRaje.1 by Associate II
  • 1079 Views
  • 1 replies
  • 0 kudos

Timer triggered ADC DMA burst only happens once

Using STM32G030F6 and STM32CubeMX, I am trying to do a sequence of single channel conversions on each edge of a PWM signal (generated by an internal timer).  PWM is setup fine and working on TIM3 channel 1.   TIM3 TRGO is set to OC1REF.  ADC is set u...

ADunc.1 by Senior II
  • 5155 Views
  • 6 replies
  • 2 kudos

lwip on STM32h743

Hello,I am using a Nucleo-h743ZI2 and would like to enable Ethernet with LWiP module. I have started with the "How to create project for STM32H7 with Ethernet and LwIP stack working" guide. I am using, with a few modifications as possible, the STM32H...

GilRoss_0-1702327149669.png
GilRoss by Associate II
  • 4861 Views
  • 3 replies
  • 0 kudos

NUCLEO-H723ZG External supply 3.3V problem

HeyI work with NUCLEO-H723ZG and I try to work with 3.3V External power supply.I try to connect the board according to the datasheet:and I saw few problems:1. My code is not working. I proggram simple code of blinking. when I work with 5V (external/u...

TOsso1_0-1703022769250.png TOsso1_1-1703023142907.png
TOsso.1 by Associate III
  • 3246 Views
  • 5 replies
  • 0 kudos

STM32H753 Ethernet initialization failure

I'm working on two custom boards using STM32H753 and DP83848 PHY. I have setup TCP communication in this setup with LwIP and RTOS and has been running in properly for the last 1.5 years. Out of the blue, in one of the boards, the TCP connection faile...

STM32H7 SPI + Level Shifter

Hi everyone,I am currently in the process of developing a board that incorporates an STM32H743VIT and a voltage level shifter (FXMA108BQX) positioned adjacent to it. The objectives are to translate 3.3V logic levels to custom voltage levels (programm...

2sayle by Associate II
  • 3739 Views
  • 2 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.