STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can RCC_LSCO be pulled to ground without issue?

Hello,We have the RCC_LSCO of the U5 connected to a peripheral that warns that it will pull this line to ground when the peripheral itself is reset. At the moment, the pull strength of this peripheral is unknown, but let's say it's fairly strong.Does...

EC.3 by Associate III
  • 1865 Views
  • 5 replies
  • 0 kudos

Resolved! Flash sector erase is taking too long

Hi all i'm developing a bootloader on a stm32f407. I want to erase all the flash sectors except of the first 3 which i have the bootloader code. The problem is that to erase a sector it takes 1 second and i have an external watchdog on the board tha...

td by Associate II
  • 6509 Views
  • 9 replies
  • 2 kudos

Sending messages using SPI peripherals - stm32f746zg

Hi, I'm using stm32f746zg board, and I need to send message from spi1(full duplex master ) peripheral to spi2( full duplex slave) peripheral (on the same board) and then back to spi1. Also i want to use interrupts/DMA.1) If the message length is unkn...

Jordalic by Associate II
  • 1726 Views
  • 1 replies
  • 1 kudos

Resolved! CAN learning

I'm interested in learning about CAN. Please suggest me any course or other tutorials to start learning

jsw2000 by Associate II
  • 2421 Views
  • 3 replies
  • 0 kudos

Resolved! What's the difference between AHB, AHB1 and AHB2?

I read in reference manual and web tutorials of stm32f103c8, there were "AHB", "AHB1" and "AHB2", what's the difference between them, I know "APB1" and "APB2" are 2 APBs, the "1" and "2" are sequential numbers, how about "AHB1" and "AHB2" are they al...

MQi.1 by Senior II
  • 7900 Views
  • 2 replies
  • 4 kudos

I2C reads FF and stucks

Hi everyone! I'm using two uC, STM32F105VCT7TR and MSP430G2452, and I'm establishong an I2C communication between them, with the STM32F105 being the master and MSP430 the slave. For the write operation, the communication works fine. However, when per...

print1.png print2.png scope_0.png
malb0794 by Associate II
  • 5820 Views
  • 12 replies
  • 0 kudos

Resolved! Regarding STM32 boards based on register and GPIO pins

 Hi,I am working in STM32F4 Discovery, in my project I want more GPIO pins but with Same registers so that  I can straight away copy  the  old programs and do programming, Is there any suggestion Please do let me know. Thanks,Mohan

MohanRaj by Associate
  • 1459 Views
  • 2 replies
  • 0 kudos

Resolved! Timer Encoder Mode, change HAL Filter after initialization

Hi all,I'm using a Timer in Encoder Mode on STM32F103, using the HAL framework on STM32CubeIDE.I would like to change encoder filter feature (IC1F[3:0]: Input capture 1 filter) depending on the behaviour selected in my MCU operation mode (so IC1Filte...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.