STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPI Communication with ATMega32

Hello,       I have to use SPI1, SPI2 and SPI3 to communicate with 3 ATmega32 boards(11MHz / 16MHz). I'm testing with STM32F407G-DISC1. My configuration and functions are as given below. void SPI3_Config(void) { GPIO_InitTypeDef GPIO_InitStru...

Rohith by Associate II
  • 3548 Views
  • 6 replies
  • 0 kudos

Nucleo board stuck when starting without USB connection

Hello,I am using a Nucleo F446RE board, and I have developped a small program that works fine as long as the board is connected to the PC with the USB cable.Once the program has been tested, I have removed the USB cable and used E5V external power su...

Jelurol by Associate II
  • 7982 Views
  • 10 replies
  • 2 kudos

Using a G4 with an Oscillator

Im planing on using a Jo22 oscillator with 24 Mhz: https://www.jauch.com/downloadfile/5ef1edcfb7fd5cebb9856be49a6932f5e/jo22-1.8-3.3v.pdf%C2%A0Are there any things i have to look out for?I havent found a example circuit, and the datasheet of the osci...

Tobe by Senior III
  • 5834 Views
  • 11 replies
  • 2 kudos

Help with modbus TCP/IP

Hello i'm currently working with the STM32F446RE and i need to implement the modbus tcp/ip protocol, im aware of the freemodbus library but i cant implement this to the stm32cubeide it is always telling me something is missing (like the port.h). It d...

GPIO_EXTI

Hi people,    I just work on a Dali project and trying to learn from the demo library I am getting some error can anyone PLEASE help me how to proceed.I am trying in STM32G0I am getting error as EXTI.Instruture undeclared i tried EXTI.Instruct but st...

SRAM.11 by Associate III
  • 2506 Views
  • 4 replies
  • 0 kudos

ST_Dalislave

Hi people,    I just work on a Dali project and trying to learn from the demo library I am getting some error can anyone PLEASE help me how to proceed.I am trying in STM32G0I am getting error as EXTI.Instruture undeclared i tried EXTI.Instruct but st...

SRAM.11 by Associate III
  • 1329 Views
  • 1 replies
  • 0 kudos

Resolved! Setting RDP option byte in STM32L452

I have a problem programmatically setting RDP to level 1.My code is:OBInit.RDPLevel = OB_RDP_LEVEL_1;OBInit.OptionType = OPTIONBYTE_RDP;ret = HAL_FLASH_Unlock();ret = HAL_FLASH_OB_Unlock();/* Clear SR register */CLEAR_BIT(FLASH->SR, FLASH_SR_BSY);ret...

SLevi.1 by Senior
  • 2889 Views
  • 2 replies
  • 1 kudos

Programming a Data in to Flash memory STM32G series

Hello Every one I am using NUCLEO-G0B1RE board when trying to store the data in to flash memory address its not updating after erasing but individually if I try only erase or only write data in to flash memory it is working please suggest me below is...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.