2019-02-07 1:42 PM
Hi guys, I've never done this before but has anyone used the onboard DACS to produce sound?
Playing a .wav file.
I know the dacs are only 12bit and it should play 8bit wave samples fine but what about 16bit samples?
I'll be receiving my MCU's next week so I can't run a test.
If anyone has done it please let me know if 12bit audio is close to 16bit audio.
Thanks guys, hope to hear from you soon.
Pete.
2019-02-07 3:42 PM
You'll need to move the 16-bit signed samples in the .WAV into the 12-bit unsigned range of DAC, obviously you'll truncate the low order precision you were holding, but the wave form will be the same, just rougher.
2019-02-07 4:43 PM
Thanks Clive. I knew I had to mask out the upper 4 bits.
Now I cant wait for my MCU's to arrive next week. Lol.
Pete.
2019-02-07 5:11 PM
Not upper but lower 4 bits.
int16_t sample;
uint32_t dac = ((sample >> 4) + 0x800) & 0xFFF;
2019-02-07 5:36 PM
The DAC has left and right aligned registers to pull the top or bottom 12-bits, what's more important is the number space conversion, and the fact the output on the DAC will have a DC offset because all the outputs will be between 0 and 3V, not +/-1.5V
From 16-bit you want to use the TOP 12 most significant bits, and lose the 4 least significant bits
if (x < -32767) x = -32767; or if (x == 0x8000) x = 0x8001; // keep within +/-32767
RIGHT ALIGNED: y = (((x + 0x8000) >> 4) & 0xFFF) or
LEFT ALIGNED: y = ((x + 0x8000) & 0xFFF0)
2019-02-07 7:39 PM
Oops, so its the lower 4 bits I have to mask out.
So I just do this ROR R0, R1, #4 /* R1 has the 16bit sample */
Unless its negative then ROL instead.
I'm an assembler guy, C wastes to many cycles for me.
Thank you guys for the help. I'll do a test next week when my hardware arrives.
Pete.
2019-02-07 8:33 PM
Not exactly, the samples are 16-bit signed, you need to adjust the zero point to get to a 12-bit unsigned range.
2019-02-07 9:49 PM
Also remember you may need an audio amplifier to produce sound: The DAC strength even with buffer might be limited.
2019-02-08 12:57 AM
Hi, Yep I 'll be using a 5v USB powered external PC Speakers. I think they're 5watts per channel.
Pete
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.