2018-03-08 7:41 AM
Hi,
Using Truestudio 9.0.0 with Nucleo STM32F302R8.
Used CubeMX to generate code.
Using ST-Link to load/ debug. Can download/ examine memory/ etc..
Use embedded COM port for debugging messages..
All works fine until I click 'Resume' followed by 'suspend'..
Then atollic_gdb_server crashes..
Seems once embedded program is running, gdb can't suspend it?
Atollic TrueSTUDIO gdbserver for ST-Link. Version 4.2.0 (WIN32 2018-01-16 10:57:14 15656)
Copyright (c) 2018, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
Persistant Mode : Disabled
LogFile Name : D:/SW_Projects/STM32_workspace/ProjectUart/Projectuart//\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
Atollic TrueSTUDIO gdbserver for ST-Link. Version 4.2.0 (WIN32 2018-01-16 10:57:14 15656)
Hardware watchpoint supported by the target
STM32 device: Flash size =65535
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x00000009
NVIC_CFGFSR_REG = 0x00000000
XPSR = 0x01000000
ST_LINK Major version =2 Jtag version =28
ST_LINK VID=1155 PID=14155
ST_LINK device status: HALT_MODE
ST_LINK detects target voltage =3.26 Volt
ST-Link device initialization OK
Waiting for connection on port 61235...
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
ST_LINK device status: HALT_MODE
Reading 0x4 bytes of memory from addr 0x8001d90
Reading 0x2 bytes of memory from addr 0x8001d8c
Reading 0x2 bytes of memory from addr 0x8001d8e
Reading 0x4 bytes of memory from addr 0x8001dc4
Reading 0x20 bytes of memory from addr 0xe00fffd0
Reading 0x2 bytes of memory from addr 0x800196c
.
.
.
ST_LINK Halt Reason break point hit
Reading 0x4 bytes of memory from addr 0x800196c
Reading 0x4 bytes of memory from addr 0x20000118
TraceCaptureStart and SWV event set to APP_TRUE
TraceCaptureStart and SWV event set to APP_FALSE
NVIC_DFSR_REG = 0x00000001
ST_LINK Halt Reason halt requested by NVIC, including step
Reading 0x4 bytes of memory from addr 0x800196e
Reading 0x4 bytes of memory from addr 0x20000118
TraceCaptureStart and SWV event set to APP_TRUE
TraceCaptureStart and SWV event set to APP_FALSE
NVIC_DFSR_REG = 0x00000001
ST_LINK Halt Reason halt requested by NVIC, including step
Reading 0x4 bytes of memory from addr 0x80002a8
Reading 0x4 bytes of memory from addr 0x8001972
Reading 0x2 bytes of memory from addr 0x8001972
TraceCaptureStart and SWV event set to APP_TRUE
TraceCaptureStart and SWV event set to APP_FALSE
NVIC_DFSR_REG = 0x00000003
ST_LINK Halt Reason break point hit
Reading 0x4 bytes of memory from addr 0x8001972
Reading 0x4 bytes of memory from addr 0x20000118
TraceCaptureStart and SWV event set to APP_TRUE
ST_LINK device status: RUN_MODE
Encountered a Socket Error, Exiting..
Debugger connection lost.
Shutting down...
Any thoughts?#
2018-04-27 3:53 AM
I'm having a similar problem. Did you ever find the resolution? Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.