2010-01-11 8:53 PM
ARM CortexM3 Compiler - Optimization
2011-05-17 4:37 AM
Any issue with CortexM3 compiling for Zero optimization?
The same code can be run with o1,o2 or o3 but cannot run with o0. Any hints? Thnx in advance.2011-05-17 4:37 AM
There is not just one ''ARM CortexM3 Compiler'' - You need to state which specific compiler and version you are using!
Quote:
The same code can be run with o1,o2 or o3 but cannot run with o0.
It is almost certainly a flaw in your source code; ie, it is relying upon something that it shouldn't, but which just happens not to fail with o1,o2 or o3. Usually it's the other way around - stuff works for no (or low) optimisation, but fails at higher optimisation. You need to do some debuggin to determine precisely what is (or is not) happening - ''doesn't run'' tells next to nothing: Check your use of volatile. Check for timing issues. Also check memory alignment issues. Are you sure that this isn't a symptom of an underlying hardware fault?[ This message was edited by: st7 on 12-01-2010 10:24 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.