2026-02-12 7:19 AM
Hello ST Community!
I am currently considering an STM32N6 for a new project and decided to use CoreMark as one of the benchmarks to compare candidates. According to its datasheet and published results on https://www.eembc.org/viewer/?benchmark_seq=13733, the STM32N657 should reach a score of ~3616. I noticed that the published results on the EEMBC website report usage of “ArmClang v15.0 - Keil v6.18” as the compiler. I figured it would be worthwhile checking what score I’d get from STM32CubeIDE’s GCC toolchain.
I ran the test on a NUCLEO-N657X0-Q board and obtained a CoreMark score of 2389, which is quite a bit lower than I expected when comparing against the published results.
The test application is designed as follows:
I confirmed that my timer (TIM2 configured at 100 MHz) and CPU clock frequency are correct using external equipment and the CM55’s DWT cycle counter.
I also tried:
But neither of those gave a better result than the initial configuration.
Are there CoreMark test scores available with ST’s own toolchain that I could compare with?
Is the “ArmClang v15.0 - Keil v6.18” toolchain really that much better than GCC at producing executable object code for the CoreMark test that it explains that large of a gap in test score?
Any additional suggestions on what should be configured to reach maximum performance?
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.