2018-11-01 1:53 PM
Hi I have configured my ADC as Input 10 bit and i would like to sample the signal from accelerometer at 20KHz. I would like to know how much of address space is the memory taking to store these? Is the memory taking 1 byte, 2 byte, 4 byte ? How can I know that in Keil/ Data sheet ?
2018-11-01 2:00 PM
Depends on the definition of the variable, C use sizeof() to determine the size in bytes of a variable, structure, array, etc.
uint16_t takes 2 bytes
uint32_t takes 4 bytes
Some fairly basic data representation stuff...
2018-11-01 2:02 PM
10-bits here could minimally use 2 bytes when stored as a 16-bit value
uint16_t array[200]; // 400 bytes
uint8_t array[1024]; // 1024 bytes
uint32_t arrary[1024]; // 4096 bytes
2018-11-02 8:44 AM
if i am using a 10 bit data from sensor, can it be stored in the format of uint8_t array ? If yes, how does the memory foot print work in this case ? will it be stored in two 8 bit addressing formats ?
2018-11-02 9:08 AM
The processor doesn't have a 10-bit format, it is held at a high precision level. The registers in the part are 32-bit, but it can also be handled as a 16-bit value
A uint16_t would be in two consecutive uint8_t memory locations, in the case of the Cortex part, in Little Endian format, so low order bits in the first byte, high order bits in the second.
An uint16_t array containing 1, 2, 3 would take six bytes in memory
01 00 02 00 03 00
This is Computer Studies 101 level stuff.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.