cancel
Showing results for 
Search instead for 
Did you mean: 

Are there any examples of the Bluetooth Advertising or Broadcasting mode of the B-L475E-IOT01A?

GStaz.1
Associate

Hello,

I am currently working with the B-L475E-IOT01A board. Through bluetooth I would like to use the mode in which I send data periodically and an external device, when it enters the transmission range, can read this data.

So I was wondering which of the Advertising or Brocasting modes is preferable to use. Are there any examples of use?

Thank You

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Ons KOOLI
Senior III

Hi GStaz.1,

Please refer to the STM32CubeL4 Firmware package.

You can find BLE applications under this directory: STM32Cube_FW_L4_V1.15.0\Projects\B-L475E-IOT01A\Applications\BLE

Best Regards,

Ons.

GStaz.1
Associate

Hi,

thanks for the reply, but I'm already using examples from that folder, but there is no example of broadcasting. I don't want the device to have authorization or to manage the connections, it just has to send data periodically and any number of devices in the range can read them.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.