cancel
Showing results for 
Search instead for 
Did you mean: 

are the external loader files for Octo SPI somewhere, github ?

MNapi
Senior III

It looks like simply replacing the QSPI loader files, which are available on github (CubeIDE)

but not all is exactly the same.

for example the are functions like

OSPI_OctalModeCfg(&hospi1);

do I need to call it somewhere ?

 

so far the loader for QSPI is working fine but OSPI is coming so far with bunch of errors.

 

 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
KDJEM.1
ST Employee

Hello @MNapi ,

ST GitHub repository contains dedicated folder for external loaders. There are many projects for ST evaluation boards and memory sales types. This GitHub provides drivers, examples, loader files and testing routines for external loaders for STM32 series of microcontrollers for QSPI and OCTOSPI.

The required steps to build a customized loader for cube programmer are available at this link (section 3.9) or in this FAQ  How to implement and use your own external flash l... - STMicroelectronics Community.

I hope this help you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I am already familiar with those projects they are done in EWARM to translate them into CubeIDE is a lot of work.

 they have the same names

like

Loader_Src.c

it does not work in CubeIDE

so there is a lot of theory to go through something I have already done.

There is tutorial from STM how to make those loader files for QSPI in CubeIDE but not for OSPI