2021-05-25 2:44 AM
I'm trying to use the internal reference voltage of 2.048V in my application, since I'm powering the microcontroller with 2.8V. But when I select the reference source and enable the VRefBuff with this lines:
HAL_SYSCFG_VREFBUF_VoltageScalingConfig(SYSCFG_VREFBUF_VOLTAGE_SCALE0);
HAL_SYSCFG_VREFBUF_HighImpedanceConfig(SYSCFG_VREFBUF_HIGH_IMPEDANCE_DISABLE);
if (HAL_SYSCFG_EnableVREFBUF() != HAL_OK)
{
Error_Handler();
}the microcontroller will go directly to the error handler. Is this because in this package the VRef is bonded to VDDA? meaning I will only be able to use VDDA as reference in this chip?
Solved! Go to Solution.
2021-05-25 3:11 AM
> Is this because in this package the VRef is bonded to VDDA? meaning I will only be able to use VDDA as reference in this chip?
This means, that you cannot use internal VREF as reference to the ADC, you have to use VDDA.
But you still can measure the internal VREF's voltage against the VDDA, thus eliminate the need to know VDDA's voltage precisely. You have to make sure VDDA is stable enough.
JW
2021-05-25 3:11 AM
> Is this because in this package the VRef is bonded to VDDA? meaning I will only be able to use VDDA as reference in this chip?
This means, that you cannot use internal VREF as reference to the ADC, you have to use VDDA.
But you still can measure the internal VREF's voltage against the VDDA, thus eliminate the need to know VDDA's voltage precisely. You have to make sure VDDA is stable enough.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.