2018-02-22 2:15 AM
hi everybody,
i 'm setting the ADC on STM32L051x6.
it works correctly but i have problem with conversion time. It is about 8us. To measure it i'm using a signal that is setted high at the start of conversion and low at the end of conversion.
The start of conversion is triggered on a timer event and i use
LL_GPIO_SetOutputPin(GPIOA, PA6);
to set signal.
I'm tryng to reduce this time.
Can somebody help me?
this is the setting code for ADC
void LED_CURRENT_ADC_Init(void)
{LL_ADC_SetClock(ADC1, LL_ADC_CLOCK_SYNC_PCLK_DIV1);
LL_ADC_SetSamplingTimeCommonChannels(ADC1, LL_ADC_SAMPLINGTIME_1CYCLE_5); LL_ADC_SetResolution(ADC1, LL_ADC_RESOLUTION_12B); LL_ADC_SetDataAlignment(ADC1, LL_ADC_DATA_ALIGN_RIGHT); LL_ADC_REG_SetSequencerChannels(ADC1, LL_ADC_CHANNEL_3); LL_ADC_REG_SetContinuousMode(ADC1, LL_ADC_REG_CONV_SINGLE); LL_ADC_ClearFlag_ADRDY(ADC1); LL_ADC_EnableIT_EOC(ADC1); LL_ADC_Enable(ADC1);}
this is the adc IRQ
void ADC1_COMP_IRQHandler(void)
{LL_ADC_ClearFlag_EOC(ADC1);
LL_GPIO_ResetOutputPin(SENS_LINEVALID_CPLD_PROGn_PORT, SENS_LINEVALID_CPLD_PROGn_PIN);
}
#conversion #adc-sampling-timeSolved! Go to Solution.
2018-02-22 6:00 AM
Take a look at the data sheet. Understand the sampling and conversion timing requirements.
It it is easy to get within 2us per manual conversion.
2018-02-22 4:17 AM
Not sure what you mean.
To measure it i'm using a signal that is setted high at the start of conversion and low at the end of conversion.
That does not matter.
In the first step, the ADC samples the external signal for the defined sampling time (by connecting it to the S&H capacitor).
Then, the S&H capacitor is disconnected from the external signal, and switched over to the internal conversion circuitry.
'Conversion time' is the number of ADC clock cycles it takes to create the digital representation of the external voltage from the S&H capacitor.
Changes of the external signal during this time are irrelevant.
I'm tryng to reduce this time.
What time, exactly ?
Conversion time is basically fixed by ADC clock and resolution.
2018-02-22 6:00 AM
Take a look at the data sheet. Understand the sampling and conversion timing requirements.
It it is easy to get within 2us per manual conversion.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.