2015-05-04 9:49 AM
Hi
I am using discovery board with stm32f429. I configured well the ADC for DMA and works fine but I don't know what is the sampling rate. Anyone can explain how to calculate it? The clock is at 90Mhz the prescaler isADC_CLOCKPRESCALER_PCLK_DIV8
samplingTime is
DC_SAMPLETIME_84CYCLES
My calculations says that sampling rate is 46875. Is that right?
Thank you in advance for any help Georges2015-05-04 10:17 AM
The sample cycles total is the programmed sample cycles plus the conversion cycles of 12, 8 or 6 depending on the conversion resolution. The DC_sample cycles is the number of cycles the sample and hold capacitor is being charged before the value is held for conversion. So the sample frequency is probably (90 MHz/8)/(84+12 cycles) = 117 KHz if you are converting continuously.
Cheers, Hal2015-05-04 11:05 PM
I made wrong calculations.
Now something else I read ,somewhere, that the ADC clock should be between 600Khz-30Mhz. This is the ABP2/Prescaler? In my case 90/8=11,25Mhz or the 117Khz sampling rate. Thank you Georges2015-05-05 6:10 AM
ADC clock frequency is defined in the STM32F427/STM32F429 Data Sheet, section 6.3.21, and lower/upper limits are 600KHz/36MHz. Other data sheet ADC performance numbers use the typical 30 MHz value. It is the frequency output of the prescalar.
One ADC clock is one sample and hold or one conversion cycle. In your example, 96 cycles are needed for one value. So your sampling frequency should be based on 96 cycles. Cheers, Hal2015-05-05 7:56 AM
Or use a timer to pace the conversion at a desired rate rather than play games with the APB, prescaler, and sample time.
2015-05-11 11:14 PM
Hi
thank you. Finally I set a timer to get the proper samplerate and works almost fine. GeorgesWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.