2014-08-08 8:29 AM
ADC resolution 12 bits(with 16 bit buffer) works but 8 bit(with 8bit buffer) results in the code going into an infinite loop in the DMA ISR.
__IO uint8_t buffer[1000];/* ADC Config*/ ADC_StructInit(&ADC_InitStructure); ADC_InitStructure.ADC_Resolution = ADC_Resolution_8b; ADC_InitStructure.ADC_ScanConvMode = DISABLE; ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T3_TRGO; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC1, &ADC_InitStructure); ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 1, ADC_SampleTime_192Cycles); #adc #stm32l1512014-08-08 8:46 AM
ADC resolution 12 bits(with 16 bit buffer) works but 8 bit(with 8bit buffer) results in the code going into an infinite loop in the DMA ISR.
Code that you conveniently fail to provide...2014-08-08 8:55 AM
I have included the code that is relevant to the problem. I don't think its a problem in the DMA_ISR. Its something in the way the ADC/Buffer works or sampling rate. ADC Is being sampled at 10KHz
void DMA1_Channel1_IRQHandler(void){ if(flag) { /*do something/* } else { /*do something else*/ } /*Clear DMA Channel Transfer Complete interrupt pending bit */ DMA_ClearITPendingBit(DMA1_IT_TC1);}2014-08-08 10:07 AM
Check the Data Alignment section in the reference manual. Byte alignment happens only for 6 bit conversions.
Hal2014-08-08 11:08 AM
Hello Hal!
Thanks for your response. Yes, I checked the ref manual and as you said only 6b and 12b can be aligned. But by default ADC_StructInit(&ADC_InitStructure); aligns by right. Also the problem does not happen when I use a 16 bit buffer. I am trying to store microphone data so would I need to do some processing to make it in PCM format or is the ADC data captured read for playback?Thanks!kj2014-08-08 11:27 AM
I have included the code that is relevant to the problem.
If you knew what code was problematic you wouldn't be here asking. Present a sufficiently complete example that can be evaluated. Most likely you aren't configuring the DMA properly, but how can I judge that? Where you clear the interrupt you'll currently tickle a Cortex-M3 hazard, you really should qualify the IT flag and clear it early.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.