2023-01-19 3:54 AM
In a stm32f303rb76, I commanded to operate ADC+DMA by setting of the
ADC DMA with circular mode
The ADC I activated continuous conversion mode
and DMA continuous request
Also the analog input signal (no scan mode)
In the initialization made following command:
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adc1_buf, 2*ADC_BUF_LEN);
Then in the debug mode I realized that always calls:
HAL_ADC_ConvHalfCpltCallback()
filling all the buffer (not a half)
But never calls to HAL_ADC_ConvCpltCallback()
it is a problem of the debugger?
How can be solved?
2023-01-20 10:10 AM
Hello @JLope.11,
Could you specify the processor frequency? the ADC frequency? clock prescaler and resolution?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.