2019-05-28 11:52 PM
I coded for usart communication in stm32f103r8.In this i'm getting the garbage value as output.
given below is my program,kindly help me to correct my program.
****
#include "stm32f10x.h"
#include "stm32f10x_usart.h"
void usartSetup (void);
int SendChar ();
int GetChar (void);
void main()
{
usartSetup();
SendChar();
GetChar();
}
void usartSetup (void) {
// make sure the relevant pins are appropriately set up.
RCC->APB2ENR |= 0x00000004; // enable clock for GPIOA
GPIOA->CRH |= (0x0BUL << 4); // Tx (PA9) alt. out push-pull
GPIOA->CRH |= (0x04UL << 8); // Rx (PA10) in floating
RCC->APB2ENR |= 0x00004000; // enable clock for USART1
USART1->BRR = 72000000L/9600L;/*115200L;*/ // set baudrate
USART1->CR1 |= 0x00000008 | 0x00000004; // TX enable,Rx enable
USART1->CR1 |= 0x00002000; // USART enable
}
int SendChar () {
while (!(USART1->SR & 0x00000080));
USART1->DR = 1;
}
int GetChar (void) {
while (!(USART1->SR & 0x00000020));
return ((int)(USART1->DR));
}
2019-06-01 5:51 AM
You should perhaps OR clock enables rather than blind write, and mask on the GPIO configurations more completely.
Review settings in debugger view of RCC, GPIO and USART1
Check signals with a scope
2019-06-02 11:21 PM
The above program is perfectly working for USART1, but if i adjust the registers for USART3 it is not working there is no signal passing. Is there any specific clock division or registers to enable.
2019-06-06 6:56 AM
Hi Sir,
As far now i researched many examples and topics related to this ,at the end i didn't get the usart initialize.
Below is my program for usart3 to Tx/Rx data. If you don't mind please validate my program and rectify it, or please send me a program for usart3.
*************
void Usart3Init(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
USART_ClockInitTypeDef USART_ClockInitStructure;
//enable bus clocks
//RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1 | RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
//Set USART1 Tx (PA.09) as AF push-pull
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
//Set USART1 Rx (PA.10) as input floating
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOB, &GPIO_InitStructure);
USART_ClockStructInit(&USART_ClockInitStructure);
USART_ClockInit(USART3, &USART_ClockInitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No ;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
//Write USART1 parameters
USART_Init(USART3, &USART_InitStructure);
//Enable USART1
USART_Cmd(USART3, ENABLE);
}
void Usart3Put(uint8_t ch)
{
USART_SendData(USART3, (uint8_t) ch);
//Loop until the end of transmission
while(USART_GetFlagStatus(USART3, USART_FLAG_TC) == RESET)
{
}
}
uint8_t Usart3Get(void){
while ( USART_GetFlagStatus(USART3, USART_FLAG_RXNE) == RESET);
return (uint8_t)USART_ReceiveData(USART3);
}
int main(void)
{
Usart3Init();
Usart3Put('A');
Usart3Put('R');
Usart3Put('M');
while (1) { }
}
2019-06-06 7:31 AM
void Usart3Init(void)
{
GPIO_InitTypeDef GPIO_InitStructure = {0};
USART_InitTypeDef USART_InitStructure = {0};
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
//Set USART3 Tx (PB.10) as AF push-pull
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
//Set USART3 Rx (PB.11) as input floating
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOB, &GPIO_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
//Write USART3 parameters
USART_Init(USART3, &USART_InitStructure);
//Enable USART3
USART_Cmd(USART3, ENABLE);
}
void Usart3Put(uint8_t ch)
{
while(USART_GetFlagStatus(USART3, USART_FLAG_TXE) == RESET);
USART_SendData(USART3, (uint8_t) ch);
}
uint8_t Usart3Get(void)
{
while ( USART_GetFlagStatus(USART3, USART_FLAG_RXNE) == RESET);
return (uint8_t)USART_ReceiveData(USART3);
}
int main(void)
{
Usart3Init();
Usart3Put('A');
Usart3Put('R');
Usart3Put('M');
while (1) Usart3Put(0x55);
}
2019-06-06 7:51 AM
This shows that Cube USART examples are yet to be application friendly.
A polling version with DMA and an interrupt version using SW FIFO would make life easier for most users.
Console ASCII demo being the default example.
Implementation of AT command handler example being a useful plus.
2019-06-08 12:23 AM
Hi Sir,
Thank you so much for your valuable concern and program. The program given by you is executing properly,but here when i try this hex file in proteus v8
i didn't get the response. Is there any function you have to make usart3 work in proteus. And one more thing is using your program i got the perfect output in usart1 in the same proteus v8.
2019-06-08 3:55 AM
Use real hardware
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.