2014-05-13 12:21 AM
Hi guys
Is there someone who knows License of ''STMicroelectronics Virtual COM Port''?Now, I'm developing a device that is included USB CDC function.It's working pretty well.In this moment, I want to apply our company's VID & PID to this driver and USB descriptor.I think it is not hard job.But I worry about License of ''STMicroelectronics Virtual COM Port''.Can i use ''STMicroelectronics Virtual COM Port'' windows driver without any license for commercial goods?If there is something which are license and processing, Please let me know. #license2014-05-13 6:18 AM
'' want to apply our company's VID & PID''
Once you change the VIP & PID - the driver that will be loaded may be different. It is up to the company developing the device to develop the install package ( the .inf file ). In any case, my understanding is the the ST VCP driver is just a wrapper for the built in Windows USB CDC default driver. The .inf file just tells Windows to use the default USB CDC device drive for the ST PID2014-05-13 9:32 AM
And also, if you modify your VCP source a little, you can use only your own inf file without ST driver. For details read:
https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fCDC%20Host%20for%20STM32F407&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy%2Es...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.