STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 voltage and current measure

Posted on May 12, 2014 at 15:19Hi All. I'm trying to use my F4 to get information from an external sensor(is a piezometer). I configure DMA+ ADC on PC1 pin and seems to work(i read something). I have same problems adn i can't figure out. 1) PC1 volt...

stm32f4 by Associate II
  • 4106 Views
  • 6 replies
  • 0 kudos

STM32F439I-EVAL2 board and STM32Cube

Posted on April 15, 2014 at 02:42We just bought an STM32F439I Evaluation board with the 5.7'' pCap touch panel/ LCD. I would like to startup a basic template project which will actually have some of the components up and running. I would like to use...

kartik by Associate II
  • 1486 Views
  • 2 replies
  • 0 kudos

BSDL file for STM32F407IG

Posted on May 07, 2014 at 16:59I am looking for a BSDL file for a STM32F407IG. The part is actually a STM32F407IGH6 Does anyone have a link where I may be able to download a BSDL for this part? Thank you

jeffrey by Associate
  • 1092 Views
  • 1 replies
  • 0 kudos

OTG FS IRQChannel not ''recognized'' by F105RBT6?

Posted on May 13, 2014 at 04:46I'm working on a project based on the V2.10 Host lib. When trying to enable global interrupt for OTG FS, the program enters the hardware fault ''loop of death''(the notorious HardFault_Handler in stm32f10x_it.c) Proble...

How do I know if the USB port (host mode) is working?

Posted on May 09, 2014 at 12:58I'm using the F105 series Stm32, and if my grab of the USB protocol being correct, the USB works on polling mechanism which means when idle, there should be regular frame of data on the DM/DP. The thing is, when I prob...

STM32F4 Discovery PIL Fails

Posted on May 05, 2014 at 16:21Hello everyone, i've been experimenting with the STM32F4 Discovery Board for quite a time now and i can get the Simulink Test Models to work (Blinking LEDs, USART Echo and so on). When i try to use any of the PIL Mode...

marc2 by Associate II
  • 1520 Views
  • 2 replies
  • 0 kudos

URB_status is always Idle

Posted on May 12, 2014 at 12:36Hi,I'm currently using the USB host library with a usb mass storage device, and it seems the host is getting stuck in the USBH_MSC_HandleBOTXfer function when waiting for the URB_Status (case USBH_MSC_SENT_CBW). Proble...

STM32F4xx_HAL_Driver documentation

Posted on March 20, 2014 at 20:52HiIm developing on the STM32F4-DISCOVERY board.I have found some HAL drivers in the STM32CubeF4 package, with lots of examples, but i'm missing a document describing how the the HAL driver should be used.Does there e...

tpb by Associate
  • 3436 Views
  • 2 replies
  • 0 kudos

FOTA

Posted on May 12, 2014 at 13:19i want to change firmware of my stm32 controller through ''Firmware over the air''.stm32 controllers have BOOT0 and BOOT1 pins for boot selection but i can not use these pins as i want to program it remotely. may any b...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.