2017-12-25 1:37 PM
Hi everyone,
I'm a fresh graduate Engineer from Egypt . I'm currently working on a project and it was decided that we will utilize the STM32F407G discovery board . The problem is that it was also decided that the Atollic truestudio lite is the IDE that we will be using as well . I have been searching far and wide and I found near to nigh of tutorials . I have been Using Microchip's PIC up until now and I'm new to the ARM as well . Do you have any suggestions as to how I should proceed?
2018-01-02 8:08 AM
>>
The problem is that it was also decided that the Atollic truestudio lite..
And who made that discussion, and why, if you need support pick a tool chain that has the level of support and visibility you and your team need.
The bulk of ST's example will build with eval versions of Keil or IAR. Or the STM32 Work Bench
Don't get stuck making bad choices, make different ones or change direction if you are going the wrong way.
2018-01-03 12:44 AM
As
Turvey.Clive.002
said, if having lots of tutorials is important to you, then you should factor that into your choice of IDE!The same applies when selecting components for your design - always be sure that you can get adequate support for your needs.
A cheap component (or tool) is useless is you can't work out how to use it!
The Atollic Lite is free - so changing to another IDE is not going to cost you...
(although note that ST has recently acquired Atollic - so things may well change...)
2018-01-03 3:08 AM
Do you have any suggestions as to how I should proceed?
Well, since you ask:
When posting questions on forums, always make the title/subject line a clear, concise, specific summary of what the thread is about.
'A new Incomer asking for some guidance' is not very informative - it probably covers about 90% of the posts here!
'Where can I find tutorials for Atollic TrueStudio?' would have been more informative.
2018-01-06 9:03 AM
Thank you very much . I misht as well do that right now !
2018-01-06 9:04 AM
That would be the project head . i came on board recently after the project direction have been sit in motion
2018-01-06 10:26 AM
This wouldn't preclude you practicing on your own computer with a different tool chain to get familiar with HAL / CubeMX on that, and then leverage that knowledge against the Atollic chain.
2018-01-07 6:37 AM
My fingers itch to write a tutorial about using the Eclipse, CubeMX plugin and the Makefile project generation, just to show it how easy and how compact the code is when using LL but we don't want to discover another error in the Jive forum, right?
2018-01-08 8:21 AM
So have you discussed with the '
project head
' about your training needs?If the project is already well-established in using this toolset, there must be co-workers who can help you?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.