2018-04-26 11:21 AM
Hi !
I have tried to follow the steps listed in/external-link.jspa?url=https%3A%2F%2Fblog.st.com%2Ftutorial-6lowpan-guide-creating-network-sending-data-internet%2F
.I got the same hardware mentioned there and I have managed to verify that I got the correct FW in my X-Nucleo IDW01M1; v160129. Finally, I have also moved the 0 ohm R4 -> R34.
However, I cannot get step 2 'Craete the Gateway' to work.I have mounted the hardware and loaded the software and when I connect to it from my PC (using Putty) I see it hanging on/********************************************************
* * * FP-NET-6LPWIFI1 Function Pack v2.1.1 * * X-NUCLEO-IDW01M1 Wi-Fi Configuration. * * WiFi Bridge Application * * * *******************************************************/ (HAL 1.7.1_0) Compiled Dec 15 2017 12:32:42 (KEIL)Board UID: 006a004f3436510b36383230Initializing the wifi module...I have reset, re-uploade dthe software with the same result.
Since there is no makefile avialable for the GW softare (STM32CubeFunctionPack_6LPWIFI1_V2.1.1), I am unable to debug it to see where it's going wrong.
So my questions are:
STM32CubeFunctionPack_6LPWIFI1_V2.1.1 gateway software so I can build it myself in System Workbench ?
Cheers & TIA !
/T
nullWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.