2008-08-13 11:34 AM
48 pin TQFP socket
2011-05-17 3:41 AM
Hi everyone,
Does anyone have a part number for a suitable socket for development use? I have managed to track down ST's part number for the 100-pin early evaluation boards but not a suitable 48 pin variant. FYI Early revisions of ST's eval boards (e.g. STM3210B-EVAL) also have a /WS part number for ''with socket'' so that when the silicon is changed, the micro can be changed easily. They are very rare after product launch. Thanks!2011-05-17 3:41 AM
I think these sockets tend to be unreliable and horribly expensive.
I think you'd be better of with one of those little TQFP-to-DIL adaptor boards from the likes of Roth, Winslow Adaptics, et al...2011-05-17 3:41 AM
Quote:
I think you'd be better of with one of those little TQFP-to-DIL adaptor boards from the likes of Roth, Winslow Adaptics, et al...
For example, here's one I prepared earlier (not TQFP, but you get the idea):2011-05-17 3:41 AM
Perhaps this will work - to our joint benefit.
My (usa) firm is building small pcbs holding STM32 (48,64 or 100 pin QFPs) small xtal, VReg, Caps, SOT Uart Level Shifter, and hi-capacity, 8 pin soic, spi eeprom. Mini JTAG and I/O connector - with optional 0.1'' adapter pcbs. Plan now is to build about 50 ea for our internal needs - can build more if the forum requests... Small qty. price is about cost of micro + 23 USD, fob usa - assembled/tested. This functional board should be less expensive than the mechanical, clamp connector you described...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.