2020-05-14 2:04 PM
The document UM1949 says:
The original firmware demonstration to reprogram the STM32 MCU of the
P-NUCLEO-IHM001, is available in binary file format from the www.st.com
website and it is called P-NUCLEO-IHM001.bin.
Also where is the source code for that firmware?
Solved! Go to Solution.
2020-05-20 12:19 AM
Thanks. I tried that. Unfortunately, the new code does not work. The motor does not start (the LED stays red). The monitor software shows Software error (FOC) error. The profiler works but it stalls a bit initially,
I am using the latest version of everything.
2020-05-21 10:19 AM
The Speedramp with Potentiometer 5.4.0 version worked with TrueStudio. Did not work with the IDE. Thanks to the input by Cedric. That helped.
2020-05-28 11:10 AM
It works with a TrueStudio compile but not with the IDE compile!!!!
2020-11-03 10:38 PM
download this file from...
All tools & software > STM32 Open Develompent Environment > X-NUCLEO-IHM07M1
en.X-CUBE-SPN7.zip will be downloaded.
finally, you can find it from...
STM32CubeExpansion_SPN7_V1.1.0\Projects\Multi\Examples\MotorControl\Binary\P-NUCLEO-IHM001\
2025-02-13 6:47 AM
Thank you very much ! You find the easiest way to solve this issue. As you said : simply download the X-CUBE-SPN7 package and copy from there the binary file. It works very very well ! I have test it and progammed with ST-Link a P nucleo IHM002 kit
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.